Skip to main content
ST Migration account
ST Community Manager
August 22, 2026
Solved

MOSFET failure & protection

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.


A P-channel MOSFET is currently used for switching the solenoid.

Case 1:
Is it possible for the MOSFET to fail?

Case 2:
If the MOSFET fails, will it become an open circuit or a short circuit?

Case 3:
If the MOSFET fails in short-circuit condition, how can the circuit be protected  

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
August 22, 2026

It is not about components from STMicroelectronics, but to help the TO, here is a suggestion for where could insert the fuse mentioned: between drain/R4 and D2/SL.

8fb91144-8b32-308b-2475-c5059197ba0b.png

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

16 replies

ST Migration account
ST Community Manager
August 22, 2026

The ignition line of the vehicle is connected to the transistor base, and the transistor collector drives the MOSFET gate. The MOSFET source is connected to the battery supply, while the drain is connected to the positive terminal of the solenoid.

In case the MOSFET fails short between source and drain, the solenoid remains continuously energized. Kindly suggest suitable protection methods for this condition.

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.
Andrew Neil
Super User
August 22, 2026

As  @Peter BENSCH  said, this sounds like just a generic electronics question - nothing to do with ST.

This is ST's forum; provided and run by ST for discussions about ST products - it's not a general electronics forum.

See this - which links to this.

 

PS:

It's far more effective to post a circuit diagram (aka schematic) than try to describe an electronic circuit in words.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.