Skip to main content
ST Migration account
ST Community Manager
August 22, 2026
Solved

MOSFET failure & protection

  • August 22, 2026
  • 16 replies
  • 94 views

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.


A P-channel MOSFET is currently used for switching the solenoid.

Case 1:
Is it possible for the MOSFET to fail?

Case 2:
If the MOSFET fails, will it become an open circuit or a short circuit?

Case 3:
If the MOSFET fails in short-circuit condition, how can the circuit be protected  

Best answer by Peter BENSCH

It is not about components from STMicroelectronics, but to help the TO, here is a suggestion for where could insert the fuse mentioned: between drain/R4 and D2/SL.

8fb91144-8b32-308b-2475-c5059197ba0b.png

16 replies

TDK
August 22, 2026

Is this a school question or an interview question?

"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Migration account
ST Community Manager
August 22, 2026

In automotive application we used to switch the solenoid in starter motor .

 

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.
Andrew Neil
Super User
August 22, 2026

 you didn't answer the question!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Peter BENSCH
ST Technical Moderator
August 22, 2026

Welcome , to the community!

Your questions are questions about the fundamentals of electrical engineering and sound like exam questions from schools.

  1. Yes, there are several reasons why the MOSFET fails
  2. The impact of the failure can depend on several things: the cause of the failure, the design of the MOSFET, the board layout, etc.
  3. For this specific case, only one fuse is necessary.

Is there a specific reason why youre asking this in a forum for STMicroelectronics devices?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Migration account
ST Community Manager
August 22, 2026

In case P Channel MOSFET get fail it become open circuit or short circuit (soruce and Drain)?

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.
Peter BENSCH
ST Technical Moderator
August 22, 2026

A fixed probability for the two cases cannot be stated without specific data. A short circuit between D-S is usually more likely in the event of overload, while an open-circuit fault is more likely if e.g. connection wires, metallisation or mechanical structures fail. The exact cause depends greatly on what the overload looks like.

In short, there can be no general answer to your question.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Migration account
ST Community Manager
August 22, 2026

85619b30-78d0-e718-a71e-27dcbd43cf9c.png

This is circuit diagram 

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.
ST Migration account
ST Community Manager
August 22, 2026

My Use of MOSFET is switch the startrer motor solenoid 

If possible shortcircuit occur in source to drain ?

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
August 22, 2026

It is not about components from STMicroelectronics, but to help the TO, here is a suggestion for where could insert the fuse mentioned: between drain/R4 and D2/SL.

8fb91144-8b32-308b-2475-c5059197ba0b.png

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
August 22, 2026

That wasn't the question - was it?

Both  @TDK  and  @Peter BENSCH  have asked you whether this is a school or interview question.

You don't seem to be using any ST products?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AScha.3
Super User
August 22, 2026

Yes.

If you feel a post has answered your question, please click on " Best Answer ".
ST Migration account
ST Community Manager
August 22, 2026

How to protect the short circuit 

 

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.
Peter BENSCH
ST Technical Moderator
August 22, 2026

As I already said: this case can be covered by a fuse, but it must be taken into account that it takes time to react.

A better approach than a p-channel MOSFET is an integrated power switch, which, in addition to a p-channel, also includes the corresponding protection functions. They are also available as high-side drivers for automotive and industrial applications.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
August 22, 2026

As  @Peter BENSCH  said, there are products specifically designed for this application - which give you protection, diagnostics, etc.

Google* "Automotive solenoid driver" or similar.

 

* other internet search engines are available

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.