Skip to main content
Associate
October 27, 2024
Question

L9907 SPI issue

Hi,

I'm configuring a L9907 Driver IC using a STM32 controller.

 The controller is sending 0xEAAA to the driver IC, however the driver IC is not responding to the input. The MISO pin is flat at 0.

Kindly help me resolve this issue

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
November 28, 2024

Whether the L9907 responds to the command depends on the programming of the STM32. But as I already mentioned in your other thread, there is no support for the industrial devices STM32 in connection with automotive devices.

The only tip I can give you: take a close look at the SPI requirements in the L9907 and initialise the SPI in the STM32 accordingly.

Good luck!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.