Skip to main content
Associate III
Dec 22, 2025 1:08 PM UTC
Question

The image from OV7670 is not displayed clearly on ILI9341

https://community.st.com/t5/others-stm32-mcus-related/ov7670-stm32f429-dcmi-dma-ili9341-spi-lcd-works-no-camera-image/td-p/864331#M9012 I am trying to display a camera image on an LCD using the STM32F429I-DISCO board, an OV7670 camera module, and an ILI9341 display.

↑This is a follow-up to my previous post.

 

However, the displayed image is extremely blurred, and it is difficult to recognize what is shown on the screen.

What should I check or adjust to display the image clearly?

IMG_1850.jpeg

1 reply

KDJEM.1
ST Technical Moderator
Jan 8, 2026 2:53 PM UTC

Hello @chachamaru;

 

Are you able to display image or color from a frame buffer?

Please look at Introduction to LCD-TFT display controller (LTDC) on STM32 MCUs - Application note application note section 7 LTDC application examples  and get inspired to check the LTDC settings.

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.