Skip to main content
Associate III
Nov 18, 2025 10:45 PM UTC
Question

STM32F303VET6 – Debugging Issues with ST-LINK V2 in IAR EWARM 9.40.2

Hello Experts,

I am using an STM32F303VET6 MCU and developing in IAR Embedded Workbench for ARM version 9.40.2.
My project compiles correctly, and debugging works perfectly when I use the I-Jet debugger.

However, when I switch the debugger interface to ST-LINK V2, I experience several issues:

  • Flash loading errors

  • Debug session failing to start

  • Random connection or SWD errors

  • In general, the application fails to debug reliably

I have verified the following:

  • The device appears in Device Manager as “STM32 ST-LINK”

  • SWD wiring and connections

  • Same board works fine with I-Jet, so hardware seems OK

Could you please advise on what additional configuration or driver settings I should check in order to make ST-LINK V2 work properly with IAR?
Any guidance would be greatly appreciated as this issue is urgent for my project.

 

Error log.

Tue Nov 18, 2025 17:43:52: IAR Embedded Workbench 9.40.2 (armPROC.dll)
Tue Nov 18, 2025 17:43:52: Loaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.2\arm/config/debugger/ST/STM32F3xx.dmac
Tue Nov 18, 2025 17:43:52: Loaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.2\arm/config/flashloader/ST/FlashSTM32F3xx.mac
Tue Nov 18, 2025 17:43:52: Connected to ST-LINK/V2 [SWD mode 1800 kHz] [Access port: 0] Firmware V2.J46.S7 (Probe no: 36FF70064D59303631062543)
Tue Nov 18, 2025 17:43:52: Hardware reset with strategy 0 was performed
Tue Nov 18, 2025 17:43:52: Initial reset was performed
Tue Nov 18, 2025 17:43:52: Loaded debugee: C:\Program Files\IAR Systems\Embedded Workbench 9.2\arm/config/flashloader/ST/FlashSTM32F3xxRAM64K.out
Tue Nov 18, 2025 17:43:52: Target reset
Tue Nov 18, 2025 17:43:56: Unloaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.2\arm/config/flashloader/ST/FlashSTM32F3xx.mac
Tue Nov 18, 2025 17:43:56: Downloaded C:\Users\dkumar\Desktop\projects-\-KEEPSAFE\Final_641_onfly-vdc - Copy\641-24sep-2mint\EWARM\Release\Exe\641-24sep-2mint.out to flash memory.
Tue Nov 18, 2025 17:43:56: 82792 bytes downloaded into FLASH (19.24 Kbytes/sec)
Tue Nov 18, 2025 17:43:56: Loaded debugee: C:\Users\dkumar\Desktop\projects-\-KEEPSAFE\Final_641_onfly-vdc - Copy\641-24sep-2mint\EWARM\Release\Exe\641-24sep-2mint.out
Tue Nov 18, 2025 17:43:56: Write failed (CPU data abort) at Memory address 0x2000'0300
Tue Nov 18, 2025 17:43:56: Write failed (CPU data abort) at Memory address 0x2000'0300
Tue Nov 18, 2025 17:43:56: Write failed (CPU data abort) at Memory address 0xe000'1028
Tue Nov 18, 2025 17:43:56: Hardware reset with strategy 0 was performed
Tue Nov 18, 2025 17:43:56: Download completed.
Tue Nov 18, 2025 17:43:56: Hardware reset with strategy 3 was performed
Tue Nov 18, 2025 17:43:56: Target reset
Tue Nov 18, 2025 17:43:56: There were 3 warnings during the initialization of the debugging session.

 

1 reply

Andrew Neil
Super User
Nov 21, 2025 11:34 AM UTC

Have you contacted IAR for support ?

https://www.iar.com/support

 

Do you have a genuine ST-Link?

How to recognize a genuine ST-LINK/V2 versus a cloned one.

 

Does the ST-Link work well with CubeIDE ?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.