Skip to main content
Associate II
Jun 11, 2025 3:59 AM UTC
Question

Standalone code for wifi Bringup

Dear sir,

We are using the STM32H747XIH6 microcontroller in our custom board, which includes Wi-Fi functionality connected via the SDIO interface. The Wi-Fi module part number is LBEE5KL1DX-883.

Could you please provide a reference source or sample code for the Wi-Fi bring-up? We are looking for a standalone application that can simply perform a Wi-Fi scan to verify the hardware functionality.

If an operating system (OS) is required for this, kindly help us with the appropriate OS source and setup steps, as we are new to STM32 MCUs.

 

 

 

Best regards,

Samudralankaiah.

This topic has been closed for replies.

3 replies

mƎALLEm
ST Technical Moderator
Jun 11, 2025 10:26 AM UTC

Hello,

Discussions on LBEE5KL1DX-883 but using STM32MP (MPUs) series:

LBEE5KL1DX-883 issue with SDMMC3

LBEE5KL1DX-883 using SDMMC3

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Jun 11, 2025 10:35 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Jun 11, 2025 10:38 AM UTC

@Samudra wrote:

we are new to STM32 MCUs.


Do you have experience with any other microcontroller(s) ?

 

Some STM32 Getting Started links:

https://community.st.com/t5/stm32-mcus-products/for-better-learning-stm32-programming-and-debugging/m-p/717799#M260260

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.