Skip to main content
MArvi.1
Associate II
Jul 7, 2022 3:44 PM UTC
Question

External Mode with STM32L476RG not working

Hi all.

I'm trying to run external mode simulation using:

  • Matlab R2022a.
  • CubeMx 6.2.0
  • STM32 Mat\Target(not sure which version)
  • Nucleo L476RG

I have created a simple LED example to test the external mode and I used the Embedded Coder to integrate it with the CubMX Project file. The problem is when i'm trying to run in external mode, I can't do it because the Monitor&Tune button is grayed out and I can't press it. In the Hardware Implementation settings, I have checked the External Mode at the Interface section. Could you guys please help me where I went wrong?

Thanks a lot.

0693W00000QKg6AQAT.png

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
Jul 7, 2022 4:14 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.