Skip to main content
KNaim.1
Associate III
Apr 21, 2025 3:09 PM UTC
Solved

Can I implement LVGL on STM32H743IIT6 with a custom LCD 1024 x 600 HD

Hello all,

I have Dev a new pcb base on STM32h743IIT6 with the below hardware:

SDRAM: 256-W9825G6KH-6

FLASH  : 25Q256JVEN

LCD: Module LCD tactile capacitif RGB IPS de 7 pouces from LCwiki buy on aliexpress
( it's a native rgb888 no driver )
Total Hardware around : 70 euro.

 

Here is the FMC and LTDC config:

SDRAM:sdram.png

 

QSPI FLASH:qspi.png

 

LTDC:ltdc.png

frame buffer.png

I have follow this post cube ide project https://github.com/JIU10/stm32h7_ltdc_dma2d/tree/master and it's work.
But now i am lost how to go further and i have some questions.
1 With the ltdc driver function below can i implement lvgl  if yes how can i do if they are some link ?

ltdc function.png

 

2 What is the best option to make and interactive lcd panel.
2 I am coming from esp32 world so I want my st32 lcd would work like famous  tftespi lib of Bodmer.

REF pcb Board rgb888 24
stm32h743rouge.pngstm32h743iit6.png






This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 21, 2025 4:52 PM UTC

LVGL is not an ST implementation. You need to contact LVGL on their forums: https://forum.lvgl.io/

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

7 replies

mƎALLEm
ST Technical Moderator
Apr 21, 2025 3:31 PM UTC

Hello,

You need to to find and read the LCD datasheet and refer to the application note AN4861 "Introduction to LCD-TFT display controller (LTDC) on STM32 MCUs" then adapt the LTDC parameters to the LCD specification or try to find if there was someone implemented it or provided its driver.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
KNaim.1
KNaim.1Author
Associate III
Apr 21, 2025 4:49 PM UTC

I have allready read AN4861 i am in this configuration
Figure 4. Display module without controller nor GRAM and with external framebuffer sdram

The lcd is working  with ltdc driver function above now i am asking how to implement lvgl

 

 

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 21, 2025 4:52 PM UTC

LVGL is not an ST implementation. You need to contact LVGL on their forums: https://forum.lvgl.io/

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
KNaim.1
KNaim.1Author
Associate III
Apr 21, 2025 6:13 PM UTC

ok forget LVGL  i will stay on ST what about touchgfx for stm32h743ii ?

mƎALLEm
ST Technical Moderator
Apr 21, 2025 7:14 PM UTC

@KNaim.1 wrote:

ok forget LVGL  i will stay on ST what about touchgfx for stm32h743ii ?


For this new question please post it on the TouchGFX forum board, sSo the dedicated team can help you.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.