Skip to main content
Associate
Feb 3, 2026 1:49 PM UTC
Solved

Bug Report: STM32F0xx_DFP 3.1.1 — Registers missing in System Viewer (Keil MDK 5.43a)

Hello ST Support Team,
I am reporting a regression issue with the latest STM32F0xx Device Family Pack (DFP) version 3.1.1 when used with Keil MDK 5.43a.
Problem Description:
Installation Issue: The DFP 3.1.1 often fails to install via the Pack Installer, showing validation errors or failing to resolve dependencies.
Missing Registers: Even when successfully installed, the System Viewer in Debug mode is empty. Peripheral registers (GPIO, RCC, etc.) do not appear for the STM32F030 series.
Environment:
IDE: Keil uVision v5.43a.0
Device: STM32F030xx (all variants)
Pack: Keil::STM32F0xx_DFP.3.1.1
OS: Windows 11
Observations:
The issue seems to be related to the new SVD (System View Description) file structure or pathing in the 3.x.x branch.
Manually pointing to an older SVD file (from DFP v2.2.3) restores the register visibility.
The "System Viewer" list in the "Peripherals" menu remains blank when using the default settings of the 3.1.1 pack.
Request:
Please verify the compatibility of the SVD files in the 3.1.1 pack with the classic Keil uVision debugger interface and check for possible pathing errors in the .pdsc file.
Best regards,
[Kent]

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Feb 11, 2026 9:02 AM UTC

Hello @Kent;

 

I tested the issue with MDK KEIL version 5.38 and STMF0xx_DFP 3.1.1 version and I can see the peripherals registers as shown in the below figures:

KDJEM1_1-1770800218765.png

KDJEM1_2-1770800435931.png

 

KDJEM1_0-1770800171730.png

 

I think the issue is related to KEIL version or KEIL installation.

Could you please try to reinstall the toolchain.

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

4 replies

KDJEM.1
ST Technical Moderator
Feb 4, 2026 8:47 AM UTC

Hello @Kent and welcome to the community;

 

Could you please try to download the svd file from STM32F0 - Arm Cortex-M0 - USB Microcontrollers - STMicroelectronics.

Then follow the steps shared in this article "How to add or update the SVD file in different toolchains: An example using Nucleo-U575I-Q board" to add the svd file in your project.

Is your issue solved?

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KentAuthor
Associate
Feb 4, 2026 5:27 PM UTC

Hello!

Problem not solved. Peripheral registers (GPIO, RCC, etc.) do not appear for the STM32F030F4P6 series.

2026-02-04 1.png2026-02-04 2.png2026-02-04 3.png2026-02-04 4.pngMDK Keil 5.38a + STM32F0xx_DFP.2.1.1 all working.

KentAuthor
Associate
Feb 6, 2026 12:51 PM UTC
Why STM32F0xx_DFP.3.1.1 has size 567kB, STM32F0xx_DFP.2.1.1 but has size 66.07mB. Maybe there is a problem in this?

 

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Feb 11, 2026 9:02 AM UTC

Hello @Kent;

 

I tested the issue with MDK KEIL version 5.38 and STMF0xx_DFP 3.1.1 version and I can see the peripherals registers as shown in the below figures:

KDJEM1_1-1770800218765.png

KDJEM1_2-1770800435931.png

 

KDJEM1_0-1770800171730.png

 

I think the issue is related to KEIL version or KEIL installation.

Could you please try to reinstall the toolchain.

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.