Skip to main content
Johan Nylund
Associate
Feb 2, 2017 11:01 AM UTC
Question

STM8AL318A peripheral registers include file

Posted on February 02, 2017 at 12:01

Hi

I am using a STM8AL318AT. What is the correct peripheral resisters include file to use? The stm8s.h includ file from the standard peripgeral library does not support any AL device. Can I use the stm8l15x.h file and uncomment the HD device?

Regards

/Johan

    This topic has been closed for replies.

    5 replies

    Oliver Beirne
    Associate II
    Feb 2, 2017 12:56 PM UTC
    Posted on February 02, 2017 at 13:56

    Hello Johan

    I have moved your question to the 

    https://community.st.com/community/automotive-mcus-community/spc5-automotive-mcus

     forum where someone should be able to assist you.

    Thanks

    Oli

    Erwan YVIN
    ST Technical Moderator
    Feb 6, 2017 10:21 AM UTC
    Posted on February 06, 2017 at 10:21

    Hello Johan ,

    Even if it could be an automotive MCUs, STM8A is relative to the arm core not PPC (SPC5 Family)

    i have put your question in STM8 Part

          Best regards

                   Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Patrice HAMARD
    Visitor II
    Feb 6, 2017 11:51 AM UTC
    Posted on February 06, 2017 at 11:51

    Hello, let me bring a little precision here. The STM8 is not based on ARM core. This is a proprietary core developed by ST. If the STMAL318AT is not described properly  (Something I will check and ask for correction), the STM8L15x will do.

    In fact we have extended the qualification and fault coverage of the standard STM8L in order to get the devices aligned with the AEC-Q100.

    Patrice 

    Max
    ST Employee
    Feb 9, 2017 11:30 AM UTC
    Posted on February 09, 2017 at 12:30

    To answer to the original question, the correct library package is

    http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm8-embedded-software/stsw-stm8016.html

    The header file is stm8l15x.h

    and the correct macro to define in the project is:

    #define STM8AL31_L_MD 

    Max

    Johan Nylund
    Associate
    Feb 9, 2017 1:00 PM UTC
    Posted on February 09, 2017 at 13:00

    Ok, thanks Max

    It sounds obvious and correct! I guess the stm8l15x.h file I got when I downloaded some LIN (STSW-STM8073/74) example did not have this macro, it was an older version.

    Regards

    /Johan