Skip to main content
Associate
March 14, 2025
Solved

STM32IDE(1.18.0) error fails to start GDB after download

Edit by ST Moderator: This post has been translated from Chinese to comply with the ST Community Terms and Conditions (§10.2).

STM32IDE (1.18.0) for the STM32F103C8T6 always fails to start the GDB after download and installation, and there is no method on the web page or official manual. Recent successes are STM32IDE (1.17.0) still working in mid to early February, and STM32IDE (1.17.0) not working at the end of February. (ST-link V2 to STM32F103C8T6)

Original:

3C8T6M32F的STM32IDE (1.18.0) 下载安装后总是无法启动 GDB,网页上的方法和官方手册也没有。最近的成功是 STM32IDE (1.17.0) 在 2 月中旬到初仍在工作,而 STM32IDE (1.17.0) 在 2 月底无法正常工作。(ST-link V2 to STM32F103C8T6)屏幕截图 2025-03-14 201237.png

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
March 14, 2025

Welcome @安和486mmk to the community!

please upload a legible photo (front and back) of the ST-LINK/V2.

The board with STM32F103C8T6 - is it a so called Blue Pill?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

12 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
March 14, 2025

Welcome @安和486mmk to the community!

please upload a legible photo (front and back) of the ST-LINK/V2.

The board with STM32F103C8T6 - is it a so called Blue Pill?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
March 17, 2025

或

1000018363.jpg

1000018364.jpg

马

TDK
March 17, 2025

Fake board, fake programmer. What could go wrong?

"If you feel a post has answered your question, please click ""Accept as Solution""."
AScha.3
Super User
March 14, 2025

See message in console : wants st-link update first !

So go menu Help -> st-link upgrade ...

then try again connect/debug .

If you feel a post has answered your question, please click on " Best Answer ".
TDK
March 14, 2025

It says you need to upgrade the STLink firmware. I would suggest starting there.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
March 17, 2025

但我已经更新了它


Google Translate:

But I have updated it

Andrew Neil
Super User
March 17, 2025

Are you sure you have that wiring correct?

AndrewNeil_0-1742226827074.png

AndrewNeil_1-1742226887940.png

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AScha.3
Super User
March 17, 2025

swd -- swc  puzzled . :D

If you feel a post has answered your question, please click on " Best Answer ".