Skip to main content
Associate
May 12, 2026 11:18 PM UTC
Solved

I need PSD311software.PSDsoft express v8.66 dosen't support programming PSD311

I need the version that support programming the PSD311,as well as the DLPortIO driver.

Thanks.

 

Andrew Neil
Andrew NeilBest answer
Super User
May 14, 2026 7:53 AM UTC

As @Peter BENSCH said, these are long obsolete and no longer supported.

https://community.st.com/t5/others-hardware-and-software/installation-problem-psd-express-866/m-p/886912/highlight/true#M46273

https://community.st.com/t5/others-hardware-and-software/psdsoft-express-and-windows-7/m-p/494435/highlight/true#M4676

https://community.st.com/t5/others-hardware-and-software/roadmap-for-psd/m-p/510117/highlight/true#M8980

 

I do remember using them back in the early 90s, when they were still Waferscale, Inc - that's over 35 years ago now!

 

BTW: Note that this is a public forum - so you might want to reconsider publishing your email address to all & sundry on the entire web ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

6 replies

Peter BENSCH
ST Technical Moderator
May 13, 2026 6:24 AM UTC

Welcome @Peanut1996, to the community!

I’m very sorry, but all devices with PSD (Programmable System Device) have been discontinued without replacement for many years now, including the associated software. You may still find something in the depths of the Wayback Machine, or a friendly user may still have something, but unfortunately STMicroelectronics can no longer help you.

Sorry that I cannot give a more pleasant answer.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Andrew NeilBest answer
Super User
May 14, 2026 7:53 AM UTC

As @Peter BENSCH said, these are long obsolete and no longer supported.

https://community.st.com/t5/others-hardware-and-software/installation-problem-psd-express-866/m-p/886912/highlight/true#M46273

https://community.st.com/t5/others-hardware-and-software/psdsoft-express-and-windows-7/m-p/494435/highlight/true#M4676

https://community.st.com/t5/others-hardware-and-software/roadmap-for-psd/m-p/510117/highlight/true#M8980

 

I do remember using them back in the early 90s, when they were still Waferscale, Inc - that's over 35 years ago now!

 

BTW: Note that this is a public forum - so you might want to reconsider publishing your email address to all & sundry on the entire web ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
May 14, 2026 8:09 AM UTC

Okay,thanks.I will keep looking.

Andrew Neil
Super User
May 14, 2026 8:15 AM UTC

You're welcome.

If you do find something, please report back - as you see, these legacy requests do come up from time to time.

Then you can mark your solution.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
May 14, 2026 8:26 AM UTC

@Peanut1996 - have you tried Rochester Electronics https://www.rocelec.com/ or similar Obsolete Component specialists?

 

Maybe also Trailing Edge Technologies: https://trailingedgetechnologies.co.uk/

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
May 14, 2026 10:59 AM UTC

I try to repair an old machine's PSD311.I've bought WSI PEP300 programmer,then I need the software.