Skip to main content
dk5ug
Associate III
Apr 12, 2004 12:51 PM UTC
Question

DK3200 applications

Posted on April 12, 2004 at 14:51

DK3200 applications

This topic has been closed for replies.

16 replies

dk5ug
dk5ugAuthor
Associate III
May 17, 2011 9:52 AM UTC
Posted on May 17, 2011 at 11:52

I give up!

My DK3200 rev0.1 obviously does not support USB.

I will not return it, but keep it so it reminds me the many hours I spent

to get it running on USB. Useless hours...

Time is running out for preparing for a seminar with some 50 ''mulitpliers''

(engineers and educators), so I prefer to stick to the old-fashioned

anchor-chip plus ATmega128 (faster and more/better A/Ds). This works.

If someone, sometime happens to bring the DK3200 to understand USB,

let me know. However, no high priority any longer.

dk5ug
dk5ugAuthor
Associate III
May 17, 2011 9:52 AM UTC
Posted on May 17, 2011 at 11:52

using DK3200 rev0.1 here

PWM to ADC DEMO v0.4 works fine

RTC-I2C DEMO Display flickers (access-timing I2C-bus? -

don't forget to place all jumpers on JP6 for this one...

USB DEMO v1.0.0 does not enumerate

USB DEMO v1.0.6 does not enumerate either and shows garbage on display

joseph2399
Associate II
May 17, 2011 9:52 AM UTC
Posted on May 17, 2011 at 11:52

There seems to be serval problems you are having with the USB interface. Please submit direct support questions to

mailto:ask.memory@st.com

and we will see if our technical support team can resolve them. Another way is to visit

http://www.st.com/stonline/prodpres/memory/psd/html/ts.htm

for specific support for the uPSD.

Thanks
dk5ug
dk5ugAuthor
Associate III
May 17, 2011 9:52 AM UTC
Posted on May 17, 2011 at 11:52

Just to give an idea where the problem is...

Enumeration works fine for the first step - until the reset.

When it comes to restart enumeration for step 2,

instead enumeration 1 restarts. Again and again and again...

Found no way to skip the reset and proceed with enumeration

step 2.

btw, in main.c UsbIsr(), RSTF is cleared. However, datasheet

says RSTF is read-only...

Of course, tried this one too

dk5ug
dk5ugAuthor
Associate III
May 17, 2011 9:52 AM UTC
Posted on May 17, 2011 at 11:52

DK3200 rev0.1 comes with R42 already removed.

LC-Display shows garbage with the USB-application note

and no USB-enumeration.

Tried Win98se an WinME.

prancergokaka
Visitor II
May 17, 2011 9:52 AM UTC
Posted on May 17, 2011 at 11:52

Try removing R42 (located behind the USB connector). I have done this and the USB demo works fine on my machine.

dk5ug
dk5ugAuthor
Associate III
May 17, 2011 9:52 AM UTC
Posted on May 17, 2011 at 11:52

I'm coming from there.

dk5ug
dk5ugAuthor
Associate III
May 17, 2011 9:52 AM UTC
Posted on May 17, 2011 at 11:52

Another try

Removed R12 (4k7 on the rev0.1 board) and replaced it by

an adjustable

Result: success with part of enumeration at a value 7k2, but

not stable

One time, the enumeration-process completed. That was, before

I removed the LM

Don't understand why the DK3200 ist detected as a full speed device,

thought this is defined as low-speed-device by the pull-up-resistor

at line USB- ...

Of course Windows-Task msgsvr32 always hangs up.

So we had ONE complete enumeration at last.

dk5ug
dk5ugAuthor
Associate III
May 17, 2011 9:52 AM UTC
Posted on May 17, 2011 at 11:52

Thank you for your help and effort.

The package looked much like the first release of the application note,

but I gave it another try of course. Same result. No enumeration.

A closer look shows, that enumeration step 1 is ok, but with the reset

ahead of enumeration step 2 the whole process restarts.

I'd like to end this discussion point - it is obvious that I am too stupid

for plug-and-play-USB.

I will investigate this problem some time later - maybe in fall.

prancergokaka
Visitor II
May 17, 2011 9:52 AM UTC
Posted on May 17, 2011 at 11:52

Hi, Please use the attachment. I have just tested it (13:15 on 24 Jan 2003)on a DK3200 rev 0.1 board, and it works fine. The attached zip file contains the Keil c files, the PSDsoftexpress files and the PC exe. I have correct operation of this software on three separate machines, 2 are win98SE and one was Win2K. My DK3200 Rev0.1 was fresh out of the box (I have previously been working on a DK3200 Rev0.0). I hope this helps.