Skip to main content
Associate
October 23, 2024
Question

Blue Pill: No STM32 Target Found

mubarak_0-1729675848217.png

 

mubarak_2-1729676325521.png

mubarak_3-1729676354416.png

 

im using STM32F103C8T6 , Im using it without any problem but yesterday i upload code , the code is not correct then i make some changes and upload again then it showing this error i use both ST-LINK UTILITY and STM32CubeProgrammer , i follow some solution in this website but is not working for me . look forwad for your reply thank you 

 

 

 

This topic has been closed for replies.

7 replies

Andrew Neil
Super User
October 23, 2024

What board is that? - give a link

and what ST-Link are you using - genuine, or a clone ?

https://community.st.com/t5/stm32-mcus/how-to-recognize-a-genuine-st-link-v2-versus-a-cloned-one/tac-p/703663/highlight/true#M965

The errors messages show that your PC is communicating with the ST-Link, but the ST-Link cannot communicate with the target microcontroller.

 


@mubarak wrote:

I'm using it without any problem but yesterday i upload code , the code is not correct then i make some changes and upload again then it showing this error


So what, exactly, did you change?

Have you disabled the pins used by the SWD connection?

https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/ta-p/49693

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
October 23, 2024

Hello @mubarak,

'X' -pill flavor boards (black, blue ) are not efficient and suffer from fake MCU. So I'm afraid, something related to the MCU itself.

I recommend you to use one of ST boards having genuine MCUs: NUCLEO-F103RB

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mubarakAuthor
Associate
October 23, 2024

im using ST-LINK V2 , i didnt disable the pins

im trying to connect PB10 and PB11 after i enable the pins i upload the code using Hex file to the STM32F103C8T6 

showing Error 

mubarak_0-1729677938021.png

 

Andrew Neil
Super User
October 23, 2024

@mubarak wrote:

i'm using ST-LINK V2


Again: is that genuine, or a clone ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mubarakAuthor
Associate
October 23, 2024

is a clone