Skip to main content
TJM
Senior II
Jun 14, 2020 10:12 PM UTC
Solved

Where can i get the download for the updated SensorTileBox firmware, SENSORTILE.BOX_v341.bin?

I captured it when the device asked for the update but the file may have gotten corrupted. Loaded v3.41 using STLinkv2 and the sensortilebox now appears to be dead. The file I have is 726691 bytes and doesn't appear to work. Sensortile won't boot, no LEDs.

thanks,

tjm

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Jun 16, 2020 1:16 PM UTC

    Well, just checked and you are right... The version I shared with you was without the Bootloader code section. Please find attached the complete FW version. Regards

    25 replies

    Eleon BORLINI
    ST Employee
    Jun 15, 2020 10:01 AM UTC

    Hi @TJM​ , are you experiencing an issue during the FOTA firmware upgrade? If this is the case, can you please tell me your smartphone model and your OS version? Btw, please check the below attachment for the SensorTile.box_V3p4p1.bin. Regards

    TJM
    TJMAuthor
    Senior II
    Jun 15, 2020 3:44 PM UTC

    Eleon, thanks for the reply. The update will not take place using FOTA. I've tried with this phone many times and It only updated one time. Never could get it done successfully since then. The phone is a Motorola G5 Plus and the OS is Android 8.1. I've had problems with other things with this phone. However, I made the update with your file this morning using the STLinkv2 and I've attached the screenshot. The line at the bottom that says 'Warning: the core is locked up' after the upload completes is a bit disturbing. With v341 installed the sensortile box is dead and locked up with no activity. I can reflash the v335 back in and it will return to normal. What's your suggestion for this? Has anyone else had issues with the v341 update. Does it require some different settings in Cube Programmer? Here is a screenshot:

    0693W000001qjxBQAQ.png

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Jun 16, 2020 1:16 PM UTC

    Well, just checked and you are right... The version I shared with you was without the Bootloader code section. Please find attached the complete FW version. Regards

    TJM
    TJMAuthor
    Senior II
    Jun 16, 2020 4:23 PM UTC

    Loaded and worked perfectly. Thanks.

    I know this unit will let the user know there is a firmware update and it will download and try to install itself but my phone just doesn't work.

    There should be a location where the firmware files can be downloaded should something get corrupted or not downloaded correctly.

    tjm

    MMade.1
    Associate II
    Jul 2, 2020 2:06 PM UTC

    Hello @Eleon BORLINI

    Is it possible to get source of current original firmware?

    I've read that this is FP-SNS-STBOX1, but when I am browsing its content, I think, it is not exactly the same, The functionality is split into several applications, am I right?

    Also the version number in the sources are 1.2.x not 3.4.1.

    I would like to just extend timestamp, they have 1ms resolution, but fastest ODR is above 6kHz, this makes recorded data not fully usable.

    Best regards

    Eleon BORLINI
    ST Employee
    Jul 2, 2020 3:15 PM UTC

    Hi @MMade.1​ , unfortunately the release of the source code of the production FW is STM proprietary and it is subject to signature of a License User Agreement (LUA); you can contact an STMicroelectronics sales office and representatives for further information. Regards

    TJM
    TJMAuthor
    Senior II
    Aug 19, 2020 12:30 AM UTC

    Eleon, v3.4.1 for the sensortile box no longer works for some reason. If I go back to v3.3.5 I have no issues the none of the v3.4.1 firmwares work. Is there a firmware more current than v3.4.1?

    niccolò
    ST Employee
    Aug 19, 2020 9:18 AM UTC

    Hi @TJM​ ,

    may I ask you how does it not work?

    Were you able to flash the code?

    Does it turn on?

    TJM
    TJMAuthor
    Senior II
    Aug 19, 2020 3:49 PM UTC

    Good morning. Thanks for the reply. This may be a duplicate reply as I'm not sure the reply from my phone actually got transmitted. Anyway, I have no problems flashing any of the firmwares to the sensortile box, but only with the STLinkv2. The update using the android app doesn't work for me. The sensortile box with v3.4.1 appears to turn on and briefly flash the LEDs when connected to power but there is no connection to the phone app. After the initial LED flash it appears to be dead and It also doesn't appear to be transmitting or receiving any signals. However, if I reflash any earlier firmware (I'm now back to v3.3.5) the unit powers up and connects quickly, perfectly and with no issues. The phone app is v4.7.1 and I believe there was an update since the last time I worked with the sensortile box. Maybe there is some incompatibility with the v3.4.1 firmware and the latest android app version.

    niccolò
    ST Employee
    Aug 20, 2020 9:47 AM UTC

    It's all right, no duplicates whatsoever.

    Anyway, have you ever read the print from the .box on a terminal (like Termite)?

    (having usb and programmer attached to the board, you should open the terminal and choose the right port)

    with that, you should be able to tell what is wrong with the initialization procedure.

    let me know if you need further help setting it up.

    TJM
    TJMAuthor
    Senior II
    Aug 21, 2020 12:01 AM UTC

    Niccolo, thanks for the suggestion. I think I've found the issue but not the actual problem.

    ST BLE Sensor v4.7.1 for Android will not connect to the sensortile.box using firmware v3.4.1

    If I drop back to firmware v3.3.5 then all versions of ST BLE Sensor for Android will work.

    ST BLE Sensor v4.6.1 WILL connect to sensortile.box with firmware v3.4.1, as well as any other firmware version, with no problems.

    It appears the issue is with the Android application ST BLE Sensor v4.7.1 . If there is some configuration that I'm overlooking to make v4.7.1 work then please let me know.

    tjm

    niccolò
    ST Employee
    Aug 21, 2020 9:58 AM UTC

    Thank you for the clarification @TJM​ , I will contact the app team and try to check where is the compatibility problem.

    I did not have this issue with my phone, so it could be telephone or OS dependent.

    Are you still using the Motorola G5 Plus with Android 8.1?

    TJM
    TJMAuthor
    Senior II
    Aug 21, 2020 5:18 PM UTC

    New development with this MotoG5Plus and Android 8.1. I've cleared all of the cache and data from the v4.6.1 app, uninstalled then reinstalled this version. This worked, as expected. I then upgraded the app to v4.7.1, rechecked the permissions then re-flashed the v3.4.1 firmware to the sensortile.box and it now appears to connect normally. I suspect that my older version of both the phone and Android left something behind during an upgrade that prevented the connection. There's no way to pinpoint the issue and it's probably not worth investing any more time for this older phone.

    Thanks,

    tjm

    niccolò
    ST Employee
    Aug 24, 2020 9:46 AM UTC

    you are welcome @TJM​ , I know that cache can become a problem when upgrading for certain phones, we are continuously looking into it and trying to fix what we can.

    Sudhir
    Associate III
    Feb 16, 2021 10:18 PM UTC

    The firmware upgrade 3.4.3 provides only SD Logging. I am using the latest version of the ST BLE Sensor app on the Android. Where can I get 3.4.x that provides the Pro functions.

    Eleon BORLINI
    ST Employee
    Feb 17, 2021 1:14 PM UTC

    Hi @Sudhir​ ,

    I see you correctly posted your query as a new request (here), so I will refer to this thread.

    -Eleon

    TJM
    TJMAuthor
    Senior II
    Mar 15, 2021 1:35 AM UTC

    Good afternoon, Eleon and/or Niccolo.

    Can you please post the latest SensorTileBox firmware here? I believe it is v3.4.3.

    Thanks,

    Tony

    Eleon BORLINI
    ST Employee
    Mar 15, 2021 12:12 PM UTC

    Hi Tony,

    now it's the v3.4.6, please find it in attachment to this comment.

    We share you the version with the Bootloader in case you use the DFU for the FW upload.

    -Eleon

    TJM
    TJMAuthor
    Senior II
    Mar 15, 2021 3:36 PM UTC

    Eleon, once again, thanks for the quick reply. Loads and runs perfectly using the STlinkV2.

    I can make a connection with the application but the BlueTooth passcodes don't appear to work, 0000 or 1234. Were these changed in the latest firmware?

    PS: Disregard the last BT issue, found my problem. 123456 .

    Thanks,

    Tony

    TJM
    TJMAuthor
    Senior II
    Mar 15, 2021 6:13 PM UTC

    Thanks, I had found that number.

    One more question. What is the designation for the battery connectors. I'd like to be able to source the connector with leads attached but I don't know the connector size or type or part number for replacement.

    Thanks,

    Tony

    Eleon BORLINI
    ST Employee
    Mar 16, 2021 8:31 AM UTC

    Hi Tony,

    It is a Molex connector: you can find the component references in THIS POST, where you can also leave a like to @SGupt.4​ who found the correct part number =)

    -Eleon