Skip to main content
MChav.13
Associate
July 12, 2019
Question

Problems with Getting Started Application b/w X-NUCLEO-GNSS and B-L475e-IOT01A1. No previous connection to the Internet is done by the B-L475e-IoT node.

The guide/documentation provided talks mainly b/w the X-NUCLEO-GNSS sensor and a NUCLEO board while I am attempting to use the L475e-IoT Node. When interacting with the application on Tera Term, the menu from the example is displayed. However, when asking to display a "position" the screen displays: "Last position wasn't valid." Moreover, the documentation requests that your IoT Node should be connected to the Internet but when rebooting the IoT Node board it never looks for a WiFi spot to connect to rather it just goes straight into the GNSS application example.

Any further directions, tips, or tutorials will be highly appreciated.

This topic has been closed for replies.

2 replies

Eleon BORLINI
ST Employee
July 15, 2019

Hi @MChav.13​ , I suggest you to share this topic in the STM32 community for the STM32L4 help and Interface And Connectivity ICs for RF and BLE support. Regards

MChav.13
MChav.13Author
Associate
July 17, 2019

Thank you Eleon. I will do so.