Skip to main content
Yair Sarid
Visitor II
July 31, 2017
Question

lsm9ds1 self test

Posted on July 31, 2017 at 12:56

Hello, I want to do a self test to lsm9ds1.

Is there any file that explain how to do it?

I found some sources  but nothing official.

If there is not official file, i have some questions:

Is the sensor can't be in motion at the time of the self test?

Is the sensor must be in specific position?

How to make self test to the magnetometer?

Thank you

Yair Sarid

#self-test #lsm9ds1
This topic has been closed for replies.

3 replies

David M.
Associate
August 31, 2017
Posted on August 31, 2017 at 09:51

Hello,

It is also not 'official' information from ST, but I am working on LSM9DS1, and for the magnetometer self-test I am using the procedure of the LIS3MDL magnetometer. The procedure I am using for the magnetometer is explained in the

/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fresource%2Fen%2Fapplication_note%2Fdm001366pdf

. Unfortunately, it is possible that the ranges for testing the results are differentbetween the

LSM9DS1magnetometer and theLIS3MDL. I asked on this forum a question about that:

https://community.st.com/0D50X00009XkXStSAN

There is also some hints in the response to:

https://community.st.com/0D50X00009XkfhlSAB

Unfortunately, as mentioned in a comment, it is not clear also for me if we have to take the difference '

NOST_DATA - ST_DATA' or'

ST_DATA - NOST_DATA'

to check the sign.

Best,

David

ST Employee
September 4, 2017
Posted on September 04, 2017 at 12:21

I'm sorry, the self-test procedure cannot be shared on the forum.

The sensor can't be in motion during the self-test.

The position during the self-test doesn't matter.

Petr S
ST Employee
September 5, 2017
Posted on September 05, 2017 at 11:52

Hello all,

david.meignan

‌ is correct, last official information confirmed that magnetometer inside LSM9DS1 is exactly LIS3MDL and you can use

http://www.st.com/content/ccc/resource/technical/document/application_note/69/d7/05/fe/a9/3e/4b/ea/DM001366pdf/files/DM001366pdf/jcr:content/translations/en.DM001366pdf

for

LSM9DS1magnetometer selftest including the limits.

Regards,

Petr