Skip to main content
Associate
Jun 3, 2025 10:03 AM UTC
Question

LSM303AGRTR are used for compass calibration bearings, but are very susceptible to interference

LSM303AGRTR 

The chip is used to calibrate the orientation of the compass, but it is very easy to be interfered with and has the following two problems

1 Calibration is very difficult to calibrate, you need to shake the sensor many times
2. After calibration is done it is very susceptible to interference, resulting in inaccurate compass data

Below is the circuit diagram, if you have a mature circuit please send me to see if there are other solutions to the problem.

FRT_ST_0-1748944885815.png


Edit by ST Moderator: This post has been translated from Chinese to comply with the ST Community Terms and Conditions (§10.2).

 

This topic has been closed for replies.

8 replies

Federica Bossi
ST Technical Moderator
Jun 4, 2025 3:11 PM UTC

Hi @FRT_ST ,

Your schematic is ok, can you explain me which issues you are experiencing?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
FRT_STAuthor
Associate
Jun 6, 2025 4:14 AM UTC

When used for compass angle calibration, it is very susceptible to interference, and the data is unstable, resulting in inaccurate angle pointing.

FRT_STAuthor
Associate
Jun 5, 2025 1:54 AM UTC

用作罗盘角度校准,非常容易受到干扰,数据不稳定,导致角度指向不准确