Skip to main content
Smalik
Associate III
October 20, 2022
Question

LIS2DH12TR- Not working on 2.9V and above voltages

Hello,

I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greater than 2.8V?

Any help would be appreciable

Thanks and Regards

Sarthak Malik

    This topic has been closed for replies.

    22 replies

    Eleon BORLINI
    ST Employee
    February 23, 2023

    Hi @Smalik​ ,

    please refer to this post --> https://community.st.com/s/feed/0D53W000025cl2NSAQ

    -Eleon