Skip to main content
Associate II
June 18, 2026
Solved

STM32U575 + ST67W611M1 hangs in W61_Net_SendData() after continuous data transmission

Hi everyone,

I am encountering an issue where my MCU freezes during continuous data transmission, and I am looking for some advice or debugging directions.

Hardware & Setup:

  • MCU: STM32U575

  • Network Module: ST67W611M1

  • Protocol: TCP

  • Driver/Firmware Version: V1.3.0

Issue Description: My application is designed to send a 1KB data packet to a remote server every 3 seconds. The transmission works perfectly fine at the beginning. However, after successfully transmitting several hundred KBs in total, the MCU gets stuck.

Through debugging, I found that the firmware completely hangs inside the W61_Net_SendData() API.

Observations:

  1. The remote server is confirmed to be alive and functioning normally when the hang occurs.

  2. The MCU does not hard fault; it simply blocks indefinitely inside W61_Net_SendData().

My Questions:

  1. Are there any known issues regarding buffer overflows or memory leaks in this specific API when sending large amounts of data over time?

  2. Is there a way to configure a non-blocking mode or set a timeout for W61_Net_SendData() to prevent the MCU from freezing?

  3. What are the recommended troubleshooting steps to find out exactly what this API is waiting for (e.g., waiting for an ACK semaphore, TX buffer full, etc.)?

Any suggestions or guidance would be greatly appreciated. Thank you in advance!

Jerrylin00Best answer
Associate II
June 26, 2026

Hi Andrew,

I realized that the SDK version I was using didn’t match.
After updating to the new version 2.0.106, I can now stably receive data exceeding 1MB.

3 replies

Andrew Neil
Super User
June 18, 2026
  1. blocks indefinitely inside W61_Net_SendData().

So have you tried stepping into that function to see exactly where & why it is hanging ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Jerrylin00AuthorBest answer
Associate II
June 26, 2026

Hi Andrew,

I realized that the SDK version I was using didn’t match.
After updating to the new version 2.0.106, I can now stably receive data exceeding 1MB.

Andrew Neil
Super User
June 26, 2026

Good news!

please mark that post as the solution  - not this one!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.