Skip to main content
DMala.1
Associate II
Sep 13, 2023 2:17 PM UTC
Solved

LVDS transceiver RHFLVDSR2D2 - Differential voltage output failure

Hello, I measure the output differential voltage of the drivers (with 100ohm termination resistor) and it is always higher than 0.4V that is referred to the datasheet. What I measure is about 0.68V. Is that normal? 

Thank you in advance

This topic has been closed for replies.
Issamos
IssamosBest answer
Super User
Sep 13, 2023 2:30 PM UTC

Hello @DMala.1 

Is this the test circuit you have used.

Screenshot_2023-09-13-15-29-45-23_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

The datasheet values are according to this test circuit.

Best regards.

II

5 replies

Issamos
IssamosBest answer
Super User
Sep 13, 2023 2:30 PM UTC

Hello @DMala.1 

Is this the test circuit you have used.

Screenshot_2023-09-13-15-29-45-23_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

The datasheet values are according to this test circuit.

Best regards.

II

Tesla DeLorean
Guru
Sep 13, 2023 2:30 PM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TDK
Sep 13, 2023 3:48 PM UTC

Was this chip supplied with 5V? In which case, all bets are off.

Unclear what the connection is between this thread and the other, or why you posted there.

"If you feel a post has answered your question, please click ""Accept as Solution""."
DMala.1
DMala.1Author
Associate II
Sep 14, 2023 7:29 AM UTC

Hello and thanks for the answers! 

The chip is supplied with 3.3V and I measure on a termination resistor of 100Ohm as in picture 3 of the datasheet, what I don't use is the two capacitors. 

Issamos
Super User
Sep 14, 2023 7:44 AM UTC

To have a credible result, you should use the same conditions as described in the datasheet (you should use the 2 capacitors).

Best regards.

II