Skip to main content
Visitor II
Aug 4, 2026 1:47 PM UTC
Question

How to configure DMA correctly with D-Cache enabled on STM32H723?

Recently, I started using the ST67W6 Wi-Fi module on a custom PCB with an STM32H723VET MCU to implement the HTTP Server application provided by ST.

The application requires D-Cache to be enabled in order to operate correctly. However, as soon as I enable the D-Cache, my other peripherals that rely on DMA transfers, such as SDMMC and ADC, stop working correctly or fail completely. When I disable the D-Cache, all of these peripherals work normally again, but the HTTP Server application no longer functions, and I am unable to detect or connect to the Wi-Fi network.

From what I have studied, I suspect that the issue is related to cache coherency between the CPU and DMA peripherals. My understanding is that I may need to configure the MPU to place DMA buffers in a non-cacheable memory region, or otherwise separate the memory used by the Wi-Fi module from the memory used by other DMA peripherals.

However, I am still learning about MPU configuration, cache management, and memory mapping on STM32H7 devices, so I would greatly appreciate some guidance on the correct approach, because I am not confident at my understanding of it as of now.

Could someone please advise on the recommended MPU/cache configuration for an STM32H723 using the ST67W6 Wi-Fi module together with other DMA peripherals such as SDMMC and ADC?

Thank you in advance for any assistance, and if I am missing any crucial information that will be needed to help me out, please inform me.

3 replies

EPASZ.1
ST Employee
Sep 25, 2026 7:03 AM UTC

Sorry for the late reply.

If it is still needed, I attach a simple project with Wifi ping functionality and ADC+DMA periodic measurement. DMA uses buffers stored inside an MPU region, so they are not affected by the D-cache.

Don’t hesitate to come back if you need more help / details.

mƎALLEm
ST Technical Moderator
Sep 25, 2026 8:20 AM UTC

Hello ​@g3nnov and welcome to the ST community,

Apart from what ​@EPASZ.1 said, need to refer to the application notes:

AN4839 “Level 1 cache on STM32F7 Series and STM32H7 Series” especially the section 3.2 Example for cache maintenance and data coherency it that explains almost the same scenario you are in.

and the AN4838 “Introduction to memory protection unit management on STM32 MCUs”

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
David Littell
Senior II
Sep 25, 2026 1:55 PM UTC

Although intended specifically for an STM32MP2xx, this article does a good job explaining the general principles applicable to all devices with DMA and a Data Cache.  I’d recommend it for study before wading into the AN’s.