Skip to main content
waclawek.jan
Super User
Aug 5, 2023 12:01 PM UTC
Solved

Please support .zip attachments

The forum allows .z, .7z, but does not allow .zip attachments.

Please fix.

JW

This topic has been closed for replies.
Laurids_PETERSEN
Laurids_PETERSENBest answer
ST Community Manager
Sep 30, 2024 11:09 AM UTC

Hello @waclawek.jan and all,

I'm happy to let you know that .zip files are now allowed in the community.

Best regards,
Laurids  

 

14 replies

RhSilicon
Lead
Aug 5, 2023 12:09 PM UTC

:see_no_evil_monkey:

Tesla DeLorean
Guru
Aug 5, 2023 12:41 PM UTC

+1

Not any more intrinsically safe / unsafe as an other archiving method, and can be scanned. Lack of support just adds to reasons not to participate.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Lina_DABASINSKAITE
ST Community Manager
Aug 18, 2023 9:06 AM UTC

Hello all, 

The type: .zip is excluded due security recommendations. Let me please check internally what could be done about it. 

BR,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
Sep 24, 2023 5:51 PM UTC

The security issue would be WHAT'S IN THE ZIP, the integrity of the files can be readily established, and the content scanned for threats.

Don't allow them to contain EXE/DLL files, or be password protected / encrypted.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Johi
Senior II
Sep 24, 2023 10:28 AM UTC

Very good proposal. On top of this the 5 MB limit is also a bit outdated. At least we should be able to share zipped example programs to support each other and indirectly ST.

Piranha
Principal III
Nov 26, 2023 7:21 PM UTC

Tried adding some files to this topic:

https://community.st.com/t5/stm32-mcus-embedded-software/how-to-make-ethernet-and-lwip-working-on-stm32/td-p/261456

Piranha_0-1701025175036.png

The RAR, 7Z, TAR and XZ archives are supported, but not ZIP because of "security". Also does any of those "security experts" even know that a DOCX, XLSX and PTPX files are also ZIP files with a different extension? @Lina_DABASINSKAITE , do you have any clue what level of nonsense you are talking here?

Oh, but it lists HEX as an accepted format - let's try that...

Piranha_1-1701025545502.png

A perfectly normal HEX files "does not match its file extension". One can see those HEX files added to that topic as a TXT files.

waclawek.jan
Super User
May 9, 2024 12:54 PM UTC

This is still a bug. As explained above, "security concern" is nonsense.

JW

Tesla DeLorean
Guru
May 9, 2024 12:59 PM UTC

.docx are ZIP files..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
Jul 27, 2024 7:07 AM UTC

@Lina_DABASINSKAITE, @Amelie ACKERMANN , can this please be rectified asap.

We need to be able to exchange packs of files. .zip is an industry standard, and, as pointed out by many, other packed formats (some of which are proprietary thus require installing/running proprietary unpackers, hence pose a significantly larger security risk) are allowed; and also formats which in fact have the same underlying .zip structure.

In other words, the quoted security concerns are moot.

We need to exchange .hex and .elf files, too - either standalone or as part of .zip  - those result from source files compilation and are vital for being able to help users with specific problems which stem from the compilation process. Those don't pose any significant security issues either, as they are not run on PCs but on microcontrollers.

JW

Amelie ACKERMANN
ST Community Manager
Jul 31, 2024 1:33 PM UTC

Hi @waclawek.jan,

I understand your point. After one year of being on the new platform, we can bring up the topic of .zip files again with the security team. However, I cannot give any promises that their assessment of the topic has changed. I will let you know if there is any news.

Best,

Amelie

Tesla DeLorean
Guru
Jul 31, 2024 6:29 PM UTC

I'm struggling to understand the "security" concern here. The files are inert, you can scan the content for things you don't want, or don't know how to decode/unpack. It's the same format used for .DOCX / .XLSX, so if I can hide and stash things in those surely those amount to the same risk?

Is the concern that bad actors might cache content you don't want to be caught hosting here?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
Jul 31, 2024 1:41 PM UTC

@waclawek.jan wrote:

The forum allows .z, .7z, but does not allow .zip attachments.


As a workaround, I think you can rename a .zip to  .z or .7z - and the forum won't notice!

:face_with_rolling_eyes:

 


@waclawek.jan wrote:

Please fix.


Yes - please fix!

After all, ST is happy enough to distribute its stuff to us as .zip !

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Laurids_PETERSEN
Laurids_PETERSENBest answer
ST Community Manager
Sep 30, 2024 11:09 AM UTC

Hello @waclawek.jan and all,

I'm happy to let you know that .zip files are now allowed in the community.

Best regards,
Laurids