Skip to main content
Andrew Neil
Super User
Feb 14, 2024 8:51 AM UTC
Question

Is there a 'Mark all as read' ?

I haven't seen a  'Mark all as read' option - am I just not looking in the right place?

ie, how to un-bold all of these - without having to open each one individually:

AndrewNeil_0-1707900612303.png

 

    This topic has been closed for replies.

    10 replies

    Laurids_PETERSEN
    ST Community Manager
    Feb 14, 2024 1:19 PM UTC

    Hi @Andrew Neil,

    The "mark all as read" function is available on board levels.
    The screenshot below is taken from the URL: 
    https://community.st.com/t5/stm32-mcus-products/bd-p/stm32-mcu-products-forum 

    mark all as read.png


    Is this a functionality you would like to have on the front page as well?

    Best regards,
    Laurids

    Andrew Neil
    Super User
    Feb 14, 2024 1:23 PM UTC

    So I'd have to go down to each board, and click it on each one?

    I think there also needs to be a Global one.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    Feb 14, 2024 1:26 PM UTC

    It says:

    AndrewNeil_0-1707917144029.png

    So that's a bit misleading - it should really say, "We marked all posts on this board as read."

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    Jan 10, 2025 10:15 AM UTC

    Any update on this?

    It remains really tedious to have to go to each board individually, then back to the main listing.

    eg, this morning:

    AndrewNeil_0-1736503868638.png

    So, to clear just 5 posts, I have to:

    1. Go to the 'Others: hardware & software' board
    2. Once there, do 'Mark All as Read'
    3. Wait for that to complete
    4. Go back to the top list
    5. Go to the 'STM8 MCUs' board
    6. Once there, do 'Mark All as Read'
    7. Wait for that to complete
    8. Go back to the top list
    9. Go to the 'STM32CubeIDE (MCUs)' board
    10. Once there, do 'Mark All as Read'
    11. Wait for that to complete
    12. Go back to the top list
    13. Go to the 'STM32 MCUs Motor Control' board
    14. Once there, do 'Mark All as Read'
    15. Wait for that to complete
    16. Go back to the top list
    17. Go to the 'MEMs (sensors)' board
    18. Once there, do 'Mark All as Read'
    19. Wait for that to complete
    20. Go back to the top list

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Lina_DABASINSKAITE
    ST Community Manager
    Jan 14, 2025 9:32 AM UTC

    Hi @Andrew Neil 

    At the moment, there’s no update on this. If something changes, I’ll let you know. 

    I let others Kudo or share their take on this idea, to see if there’s a bigger need for such an improvement.

    Regards,
    Lina

    ​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.