WATCH ON-DEMAND | STM32 Summit 2026
Raise questions or provide feedback on our community platform.
Most recent activity
When looking at a subforum, on the right side there are many labels available. For example, for the "Embedded software (MCUs)", the list starts with a label "ADC". But, when creating or editing a topic, there are just 9 labels available starting with "STM32Cube MCU Packages". Adding a valid label manually, ends up with an error message: "The following labels are not available here: ...".
This is not a bug of the forum engine, but of the main ST web server! Let's open the following link:https://www.st.com/resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdfBy default on a Chromium/Blink based browsers it just opens a PDF file in a tab, but on Firefox it offers a file download. The cause of the difference is the HTTP Content-Disposition header. Look at what a valid syntax is and what the ST web server returns:content-disposition: /resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdfThis is a nonsense, which doesn't conform to the HTTP standard! Apparently the Chromium/Blink based browsers interpret such a nonsense as "inline", but the Firefox interprets it as "attachment". Read the following link for a more detailed explanation and an override workaround for Firefox:https://support.mozilla.org/en-US/questions/1387228
If one takes a link to a specific post, then the posts, which had been moved from other topics, show the title of their respective original topic.Original post (OK)Moved post (wrong title):Also, as I have reported previously, adding a "Re: " in front of the title, is an anachronism from the e-mail "traditions" and is not only useless, but also worsens the usability.
I hate when i have to come on this site for resources.Now i need to download https://www.st.com/en/embedded-software/stsw-wise-studio.htmlBut it just does'nt work as i keep being repeated I have to log in but i already am. I tried switching browser.Nothing works, and i've lost so much time already :(Stress and money loss for me, thank you.
Hi, Just wondering what happened to the "My Creations" where people could post entire projects? I have a couple of projects that solve some of the problems people have had such as WiFi for the STM32H7B3I-DK, using one pulse timers, and have posted one or two projects in the past, but they have disappeared.Best regardsRob
Pictures got lost during migration, too, for example: JW
I would like to change my account password, but I can't find how to do it...Under my account and my settings I can't find any option/command for this purpose.
https://community.st.com/t5/stm32-mcus-products/uart-receive-issue/m-p/602914/highlight/true#M226105How am I supposed to view a code at a longer lines, which have to be scrolled to the right, if the horizontal scrollbar is 8 screens down? And such a long blocks are not usable anyway. There is a simple solution for both of these issues - limit the maximum vertical size of the code blocks. The size should definitely be smaller than the average screen size. Probably some 30-40 visible lines of code are fine.
Duplicating posts, uploading the same files multiple times, even replying to themselves - nothing will stop "alternatively gifted" users from abusing that button and creating a mess.https://community.st.com/t5/stm32-mcus-products/stm32f4-hardfault/m-p/604656/highlight/true#M226598The whole idea of "in response to ..." is a leftover from the broken threaded mode design. The Reply button on every post, the "in response to ..." line and the whole threaded mode should be removed and instead a proper actually useful quoting should be implemented.
and have certain freedom of speech here? ))
To add insult to injury, in preview, the text is not shortened:I strongly suggest to invite Khoros' "experts" to experience the shame personally here.JW
Every day some alternatively gifted user creates a duplicate topics, people often comment on more than one of those and in the end the information is scattered in around and is a mess. For an example:https://community.st.com/t5/stm32-mcus-embedded-software/regarding-software-package-for-nucleo-f070cb-in-stm-cube-ide/td-p/604679https://community.st.com/t5/stm32cubeide-mcus/regarding-mcu-package-for-nucleo-f070cb-in-stm-cube-ide/td-p/604695The question: Can the moderators merge such topics, if those are reported? I know it can be done in real forums, but can this pseudo-forum system do it?P.S. Users should receive some light punishment for creating duplicate topics, posts or anything.
Open this link in Firefox:https://community.st.com/t5/stm32cubeide-mcus/cubeide-forcing-you-to-login-to-st-is-complete-bull-excrement/m-p/584715/highlight/true#M20219
This used to be possible.
Dyslexic reference to SMT32https://www.st.com/en/microcontrollers-microprocessors/stm32f469-479.html"The STM32F469 and STM32F479 lines deliver the highest Arm® Cortex®-M4 performance and embed large memories and rich peripherals to enable the most advanced consumer, industrial and medical applications. The ART Accelerator™ for Flash memory and the Chrom-ART Accelerator™ for graphics coupled with LCD-TFT and MIPI-DSI display interfaces enables an advanced user interface while granting enough resources for demanding real-time processing.The STM32F469 and SMT32F479 product lines provide from 512 Kbytes to 2 Mbytes of Flash, 384 Kbytes of SRAM and from 168 to 216 pins in packages as small as 4.89 x 5.69 mm."
I unsubscribed from all of the ST marketing in 2021-Apr-21 (one can see the confirmation e-mail at the bottom of the screenshot), but since 2022-Nov-29 I am receiving it all again.Checked the communication preferences in my profile at ST.com - my previous settings (before the 2021-Apr-21) have returned. What is ST's excuse this time?
Hello to everyone I have to check a bulk ID Exist a specials page or link to do that?
Is there a general statement on PFAS for ST Micro products? If not, can you advise if parts attached contain PFAS?
I used drag-and-drop from a highlighted text in other's post to the editor pane, after which the whole page remained shaded out, including the "reply" button, to which I can't click.Typing in the edit pane still works, but can't do anything other than reload.#javascriptoid_messJW[EDIT] After dropping a random *file* into the area marked as "drag and drop file" the page "unfroze".
ST is removing their posts, but not removing the profiles:@unknown@unknown@unknownAnd in some cases the opposite has been done - the profile has been removed, but the posts hasn't:https://community.st.com/t5/stm32-mcus-products/can-t-get-adc-values/m-p/50756/highlight/true#M50
This is my complaint about the st.com website. This site is a usability nightmare.It is completely spammend with trackers and analytics, loading tons javascript from almost everywhere, it became practically unusable.e.g.: I needed almost 30 minutes to find a deep link to the current version of the CubeIDE windows installer. The CubeIDE landing page is bloated by such an extent with tracker and analytics javascript, blocking each other, if one is blocked by my brower, i was litteraly not able to click on the download button, because it vanished after logging in.Pardon my french, but this sucks completely. I understand you want to do analytics, but if the user blocks those trackers, because of trust issues, then the site should work without them.Thank you for your attention</rant>
I was just told that I've reached a limit of 1000 uploaded images.Now what?JW
... can be written, but can't be sent:JW
Hi, how to fix these error 'ai_layer_conv2d' {aka 'struct ai_layer_conv2d_'} has no member named 'in_ch_format' and 'ai_layer_conv2d' {aka 'struct ai_layer_conv2d_'} has no member named 'out_ch_format' after clicked Project > Clean... ?
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.