Skip to main content
Piranha
Principal III
Oct 31, 2023 1:54 AM UTC
Question

Code blocks are too long

https://community.st.com/t5/stm32-mcus-products/uart-receive-issue/m-p/602914/highlight/true#M226105

How am I supposed to view a code at a longer lines, which have to be scrolled to the right, if the horizontal scrollbar is 8 screens down? And such a long blocks are not usable anyway. There is a simple solution for both of these issues - limit the maximum vertical size of the code blocks. The size should definitely be smaller than the average screen size. Probably some 30-40 visible lines of code are fine.

This topic has been closed for replies.

2 replies

Lina_DABASINSKAITE
ST Community Manager
Nov 3, 2023 11:08 AM UTC

Hi Piranha, 

Thanks for the feedback provided! I will check what options to we have to adjust to the requirements and get back to you. 

Thanks a lot, 
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Piranha
PiranhaAuthor
Principal III
Nov 10, 2023 12:16 AM UTC

https://community.st.com/t5/stm32-mcus-products/can-dma-trigger-mdma-block-transfer-linked-list/td-p/603854

Even a better example - select a superlong post as a solution and you get two superlong posts... :face_with_tears_of_joy: