Skip to main content
Associate II
Dec 11, 2024 7:53 AM UTC
Solved

ST Edge AI Developer Tool: Onnx IR version error, Matlab

Hello everyone,


I am trying to use the ST Edge AI Developer Tool and I am encountering the following error when I try to quantize my model (a RNN with an input layer, 3 GRU layers and a Fully Connected layer):

 

 2024-12-11 07:25:35.451880: I tensorflow/core/util/port.cc:113] oneDNN custom operations are on. You may see slightly different numerical results due to floating-point round-off errors from different computation orders. To turn them off, set the environment variable `TF_ENABLE_ONEDNN_OPTS=0`. 2024-12-11 07:25:35.479788: I tensorflow/core/platform/cpu_feature_guard.cc:182] This TensorFlow binary is optimized to use available CPU instructions in performance-critical operations. To enable the following instructions: AVX2 AVX512F AVX512_VNNI FMA, in other operations, rebuild TensorFlow with the appropriate compiler flags. ONNX Runtime Model Optimization Failed! Consider rerun with option `--skip_optimization'. Traceback (most recent call last): File "/usr/local/lib/python3.9/site-packages/onnxruntime/quantization/shape_inference.py", line 91, in quant_pre_process _ = onnxruntime.InferenceSession(input_model_path, sess_option, providers=["CPUExecutionProvider"]) File "/usr/local/lib/python3.9/site-packages/onnxruntime/capi/onnxruntime_inference_collection.py", line 347, in __init__ self._create_inference_session(providers, provider_options, disabled_optimizers) File "/usr/local/lib/python3.9/site-packages/onnxruntime/capi/onnxruntime_inference_collection.py", line 384, in _create_inference_session sess = C.InferenceSession(session_options, self._model_path, True, self._read_config_from_model) onnxruntime.capi.onnxruntime_pybind11_state.Fail: [ONNXRuntimeError] : 1 : FAIL : Load model from /tmp/quantization-service/3e006691-c53a-4aca-bf0e-804efdb92544/RNN_Final_FT.onnx failed:/onnxruntime_src/onnxruntime/core/graph/model.cc:147 onnxruntime::Model::Model(onnx::ModelProto&&, const PathString&, const IOnnxRuntimeOpSchemaRegistryList*, const onnxruntime::logging::Logger&, const onnxruntime::ModelOptions&) Unsupported model IR version: 9, max supported IR version: 8


My network is exported from MATLAB 2024b in a ONNX file. Does anyone know how to fix this error?

Thank you in advance!
Silvia

This topic has been closed for replies.
silviagBest answer
Associate II
Dec 11, 2024 9:43 AM UTC

Hello @Julian E. 

Thanks for the help. I can confirm that the solution suggested here Solved: Which Intermediate Representation Version needed -... - STMicroelectronics Community works perfectly also in my case. Thanks again!!

Have a good day,
Silvia

3 replies

Julian E.
ST Technical Moderator
Dec 11, 2024 9:12 AM UTC

Hello @silviag ,

 

A user had a similar issue, here is what he said in the end:  

I found a simple fix - I installed Matlab R2024a and did the export with it (ir version = 7) - that works great.

 

The thread: Solved: Which Intermediate Representation Version needed -... - STMicroelectronics Community 

 

Have a good day,

Julian

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
silviagAuthorBest answer
Associate II
Dec 11, 2024 9:43 AM UTC

Hello @Julian E. 

Thanks for the help. I can confirm that the solution suggested here Solved: Which Intermediate Representation Version needed -... - STMicroelectronics Community works perfectly also in my case. Thanks again!!

Have a good day,
Silvia

silviagAuthor
Associate II
Dec 11, 2024 9:57 AM UTC

Hello again @Julian E. 

If I quantize without a representative data set, the quantization is successful. But if I try to quantize loading my data set, I obtain the following error: "Initializer gru_1_Gather1Indices appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py." that is seemed to be repeated for the entire structure of the model (see below).

Do you have suggestions?

Thanks,
Silvia

Executing with: {'model': '/tmp/quantization-service/3512eb56-41a5-4055-a2ee-82ec3ea3b21c/RNN_Final_FT_01.onnx', 'data': '/tmp/quantization-service/3512eb56-41a5-4055-a2ee-82ec3ea3b21c/dataForQuantization.npz', 'disable_per_channel': False}
Preprocess the model to infer shapes of each tensor
Quantizing model...
[ONNXRuntimeError] : 2 : INVALID_ARGUMENT : Invalid rank for input: sequenceinput Got: 1 Expected: 3 Please fix either the inputs or the model.

2024-12-11 09:45:15.150815: I tensorflow/core/util/port.cc:113] oneDNN custom operations are on. You may see slightly different numerical results due to floating-point round-off errors from different computation orders. To turn them off, set the environment variable `TF_ENABLE_ONEDNN_OPTS=0`.
2024-12-11 09:45:15.178400: I tensorflow/core/platform/cpu_feature_guard.cc:182] This TensorFlow binary is optimized to use available CPU instructions in performance-critical operations.
To enable the following instructions: AVX2 AVX512F AVX512_VNNI FMA, in other operations, rebuild TensorFlow with the appropriate compiler flags.
2024-12-11 09:45:16.353965760 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_1_Gather1Indices appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.353993394 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_1_ConcatConst1 appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.353999607 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_1_initial_h appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354005795 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_1_W appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354012106 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_1_R appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354017159 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_1_B appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354022133 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_2_Gather1Indices appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354027241 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_2_ConcatConst1 appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354032237 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_2_initial_h appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354037797 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_2_W appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354043986 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_2_R appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354049898 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_2_B appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354055581 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_3_Gather1Indices appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354060986 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_3_ConcatConst1 appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354066310 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_3_initial_h appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354070950 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_3_W appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354075668 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_3_R appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
2024-12-11 09:45:16.354081578 [W:onnxruntime:, graph.cc:1231 Graph] Initializer gru_3_B appears in graph inputs and will not be treated as constant value/weight. This may prevent some of the graph optimizations, like const folding. Move it out of graph inputs if there is no need to override it, by either re-generating the model with latest exporter/converter or with the tool onnxruntime/tools/python/remove_initializer_from_input.py.
....