Solved
ML Model Input Buffer problem
- 3 replies
- 1522 views
Hello,
I am working on a NUCLEO-N657X0-Q and i'm trying to fill the runtime input buffer of an NPU accelerated miniresnet model with random data in order to verify that it is working, however, the buffer remains unaffected and filled with zeroes.
Do I have to do something different before/after filling (like invalidate some kind of cache?)
I am attaching a snippet of the code and the UART output aswell as the model analysis text.
I am using the external flash to store the model @ 0x71000000 (n6-extflash profile). The npuRAM5 (0x342e0000) is also used and project is setup as LRun.
The base code was generated by STM32CubeMX GUI
Thanks
Tasos