Skip to main content
Lina_DABASINSKAITE
ST Community Manager
Jul 18, 2023 8:31 AM UTC

Help others to solve their issues

“Best answer” is much more than a simple green checkmark next to a subject. They are instrumental in helping community members find answers to their questions faster and more effectively. The “Best answer” mark also helps community members move up the ranks in the ST Community and become known as true experts in their field.

Here is how you can use “Best answer” to reward community members who have helped you and contribute to the growth and quality of the ST Community, benefiting all members, including yourself:

  1. Post your question in the community following the instructions from our “How to Post” tutorial.
  2. Wait for a reply from one of our experts, a community member, or an ST employee.
  3. Continue the conversation if needed until a solution is found.
  4. Once your initial question has been answered, click on "Best answer" on the post, which solved your issue or answered your question:

 

 

 

Threads marked as “Best answers” stand out from the discussion threads and help you and others find a solution more easily:

 

 

 

If you accidentally choose the wrong post as the solution, you can revert this action by clicking Unmark answer and selecting the correct one again: 

 

 


Important:

  • The actions "Best answer" and "Unmark answer" are restricted to the author of the post and community moderators only. 
  • After your initial question is resolved, please start a new post for any additional questions instead of adding them to the same conversation.
  • If you encounter any issues, please “Report” your post with a brief explanation, and the forum moderators will take the respective action. 
     

     

Thank you for helping us make the ST Community an even better place to get answers and solve issues.

    6 replies

    Andrew Neil
    Super User
    Jul 5, 2024 1:02 PM UTC

    @Lina_DABASINSKAITE wrote:


    4. Once your question has been fully answered, click on "Accept as Solution" on the post, which solved your issue or answered your question


    If there isn't a single post which solved your issue or answered your question, then write a post which summarises the solution - and mark that post as the solution.

    Yes, you can mark one of your own posts as the solution.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Tesla DeLorean
    Guru
    Jul 5, 2024 2:03 PM UTC

    I do find this One Question / One Answer model highly flawed. Most of the time there's a focus on the wrong thing, and problem solving is about getting to the details and the actual issue, and frequently not the symptoms.

    >>If there isn't a single post which solved your issue or answered your question, then write a post which summarizes the solution 

    Personally, I'd like to see this in any case to get some closure, and up voting the best answer(s) that led to a solution.

    >>and mark that post as the solution.  Yes, you can mark one of your own posts as the solution.

    I'm not a fan of this, unless none of the responses were on-point or on the path to the final answer/solution

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Andrew Neil
    Super User
    Jul 5, 2024 2:27 PM UTC

    >> I'm not a fan of this, unless none of the responses were on-point or on the path to the final answer/solution

    It's most useful when the OP finds their own solution - possibly before anyone else has replied.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    BarryWhit
    Lead
    Jul 5, 2024 3:25 PM UTC

    > It's most useful when the OP finds their own solution - possibly before anyone else has replied.

    on at least one occasion, after I took some pains to provide a detailed answer, the OP created a new post which simply repeated the detailed solution I suggested, then added a single step which was not necessary according to the original question, and finally accepted their own solution. I did not appreciate this - I thought it was quite rude. There wasn't even a thank-you.

     

    On another occasion, the question was "How do I do X?", and the answer was "You can't do X". However, since this is not the answer OP was looking for, they simply ignore it, or try to "bargain" their way around impossibility. In such cases, the helpful thing to do is to hold their hand while they emotionally process their disappointment. Like Delorean says, this is quite common.

    "- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."
    Tesla DeLorean
    Guru
    Jul 5, 2024 4:01 PM UTC

    >> I did not appreciate this - I thought it was quite rude. There wasn't even a thank-you.

    Yes, forums can be a thankless place, with a lot of expectations. I wouldn't take this personally, but it is pervasive and depressing.

    Unfortunately how the metrics and scoring work here tend to reinforce the bad experience for those who contribute to answers and content. I have little confidence that this will change.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    BarryWhit
    Lead
    Jul 5, 2024 4:19 PM UTC

    *withdrawn*

    "- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."