Skip to main content
srosen
Associate
November 19, 2014
Question

Using CAN on SPC560B-DIS

Posted on November 19, 2014 at 16:24

Hello,

I am trying to make a simple project that for a start can send a single CAN frame.

I am using the SPC560B-DIS evb without any CAN board (will connect later on my own converter).

I took a CAN sample  from other evb and merged it to my project but it doesn't work!

Is there any CAN sample that works that I can use?

Can I connect a scope to the TX pin and view the data without converter to CAN High and CAN Low?

In the example i did not see any initialization to the I/O (Tx and Rx) is that correct?

Can I use the external clock on my board for the CAN module?

Thanks

Shachar
    This topic has been closed for replies.

    11 replies

    Erwan YVIN
    ST Technical Moderator
    November 19, 2014
    Posted on November 19, 2014 at 17:25

    Hello Rosen ,

    Do you succeed to take the hand by JTAG USB and PLS?

    There is an application for motherboard & mini-module

    SPC560Bxx OS-Less CAN Test Application

    You can use like starting point these application (importing from Appwizard)

    SPC560Bxx OS-Less Test Application for Discovery

    Take the CAN configuration of SPC560Bxx OS-Less CAN Test Application

    and use these configurations into SPC560Bxx OS-Less Test Application for Discovery

    WARNING : the io settings are different and the clocks settings are completely different

    otherwise you should not boot.

    Anyway , we will update the application repositories in the following weeks especially for discovery boards.

    yes , it is possible to connect to the TX pin and view the data

    compare SPC560B6DIS I/O headers with your reference manual.

    CAN peripheral is started by canStart.

    for the CAN module , you can use an external clock by settings your low level drivers option.

    Best regards

    Erwan

    ________________

    Attachments :

    2014-11-19_172054.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qW5u&d=%2Fa%2F0X0000000bo4%2FEnbKO0oN0Q2qgoSvrFzC5hpPT3WMg2w5C4w_Hl7EzPM&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    srosen
    srosenAuthor
    Associate
    November 20, 2014
    Posted on November 20, 2014 at 10:25

    Hello Erwan,

    Thanks for the quick response.

    I did manage the JTAG USB and PLS, took me a while but it works now.

    Regarding your suggestion,  that is exactly what I did yesterday but no luck with it.

    question:

    1. Why isn't there any CAN I/O defined in the example? Shouldn't it be configured in the configuration file just like the Leds and the Push button?

    2. Is there an option to use C++ compiler during the evaluation period?

    Thank you,

    Shachar

    Erwan YVIN
    ST Technical Moderator
    November 20, 2014
    Posted on November 20, 2014 at 14:35

    Hello Rosen ,

    1) About CAN driver ,

        the 8 first mailbox id are dedicated for RX (canReceive) (Input)

        the 8 next mailbox id are dedicated for TX (canTransmit) (Output)

        the component GUI (on CAN) is used to enable , disable and configure your CAN Drivers.

        The test application is to send a CAN Message on a channel with EID 0x1234567

    2) We are using a ''gcc powerpc vle'' provided by hightec.

         there is no option to use the C++ compiler.

         it is existing in our plugin :

         c:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.hightec_1.0.0.201306281422\hightec\bin\ppc-vle-g++.exe

         you have to create and update your platform component to provide the compilation on c++

     Best Regards

                           Erwan

    Hello Erwan,

    Thanks for the quick response.

    I did manage the JTAG USB and PLS, took me a while but it works now.

    Regarding your suggestion,  that is exactly what I did yesterday but no luck with it.

    question:

    1. Why isn't there any CAN I/O defined in the example? Shouldn't it be configured in the configuration file just like the Leds and the Push button?

    2. Is there an option to use C++ compiler during the evaluation period?

    Thank you,

    Shachar

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    nooshin_1382
    Associate III
    January 7, 2015
    Posted on January 07, 2015 at 14:10

    Hello Rosen

    I have the same problem i wrote the code and compile it successfully but no action on Tx CAN Pin

    is your problem solved ?

    if you know what is the problem please help me on this

    thanks

    Best Regards

    vanima

    Erwan YVIN
    ST Technical Moderator
    January 16, 2015
    Posted on January 16, 2015 at 15:25

    Hello Vanima ,

    I have no problem :

    About the current CAN driver , 

        the 8 first mailbox id are dedicated for RX (canReceive) (Input) (1,2,3,4,5,6,7,8)

        the 8 next mailbox id are dedicated for TX (canTransmit) (Output) (9,10 ....16)

        Tx Channel ID 1 means 9 (in lld part) ....and so on ..

    Next Week, There is will be a improvement on CAN driver on the version 3.4.0

    #281492 CAN Naming convention : Change the id number of Filter

    #286966 The message buffers Tx/Rx Configuration in CAN module 

    will be dynamic

      Best regards

            Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    souha
    Associate
    April 2, 2015
    Posted on April 02, 2015 at 13:27

    Hello,

    I'm trying to send a CAN message on SPC560 B discovery board  using chibi OS.

    I configured the CAN1 Tx pin (PC10) and Rx pin (PC11) and connect it to an external CAN transceiver. I m using  ''cantransmit ''function available (canTransmit(&CAND2, 3, &txmsg, TIME_IMMEDIATE). I can't see any signal in CAN pins.

    Have you any idea about the possible problem? Have you a sample code to test CAN using chibiOs on SPC560B-dis?

    Erwan YVIN
    ST Technical Moderator
    April 7, 2015
    Posted on April 07, 2015 at 17:22

    Hello Souha ,

    Did you try to adapt the configuration for ''SPC560Bxx OS-Less CAN Test Application'' ?

    For this application , you have just to change the clock settings.

    we have created a Change request for to pout in the Application Wizard some new applications for ''SPC560Bxx for discovery''.

       Best Regards

                     Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    souha
    Associate
    April 9, 2015
    Posted on April 09, 2015 at 12:48

    Hello Erwan,

    I m a little confused with clock settings(system clock or CAN clock). Which settings did you  put?

    Thanks for help

    Souha

    Erwan YVIN
    ST Technical Moderator
    April 29, 2015
    Posted on April 29, 2015 at 17:47

    Hello Souha ,

    The application ''SPC560Bxx OS-Less CAN Test Application for Discovery'' is in attachment.

    it will be integrated in the next release.

    best regards

    Erwan

    ________________

    Attachments :

    SPC560Bxx_OS-Less_CAN_Test_Application_for_Discovery.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qVYC&d=%2Fa%2F0X0000000bny%2F68hJTIcxfG4eyWwuchEup6CyKlbiZy37ccZ3wVa0.YI&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    sdesance
    Visitor II
    October 14, 2015
    Posted on October 14, 2015 at 11:46

    Hello Erwan,

    I have the same question than other people in this post.

    I want to use a CAN port with the SPC560B-DIS.

    I have donloaded the ''SPC560Bxx OS-Less CAN Test Application for Discovery'' configuration that you have given in your last post and I try to configure it for use the FlexCAN0 module: I disable loopback mode, but I can't see anyt signals with my scope on TX and RX ((PB[0] and PB[1]).

    My application is in attachment: can you say me what is wrong?

    Thanks for your help,

    Sylvain

    ________________

    Attachments :

    MX_SPC560Bxx_OS-Less_CAN_Test_Application_for_Discovery.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qZEp&d=%2Fa%2F0X0000000bp9%2FmP742HZNDYQBe9mNU8.KVIg6GPVjANfCJfai5ThgsGA&asPdf=false