Skip to main content
srosen
Associate
Nov 19, 2014 3:24 PM UTC
Question

Using CAN on SPC560B-DIS

Posted on November 19, 2014 at 16:24

Hello,

I am trying to make a simple project that for a start can send a single CAN frame.

I am using the SPC560B-DIS evb without any CAN board (will connect later on my own converter).

I took a CAN sample  from other evb and merged it to my project but it doesn't work!

Is there any CAN sample that works that I can use?

Can I connect a scope to the TX pin and view the data without converter to CAN High and CAN Low?

In the example i did not see any initialization to the I/O (Tx and Rx) is that correct?

Can I use the external clock on my board for the CAN module?

Thanks

Shachar
    This topic has been closed for replies.

    11 replies

    Erwan YVIN
    ST Technical Moderator
    Oct 15, 2015 9:42 AM UTC
    Posted on October 15, 2015 at 11:42

    Hello Sylvain ,

    i do not see any filters on your CAN configuration.

    How do you check your CAN Frame transmission ?

        Best Regards

                          Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.