Skip to main content
Rohit Rajapure
Associate III
Nov 20, 2023 7:34 AM UTC
Question

SPC582Bxx CAN initialization and configuration

Hello All, 

we are using the SPC582Bxx family device for our automotive system, 

We have gone through the guides related to SPC582Bxx, Auto devkit studio and ran some sample code by referring the tutorial available from ST team. 

since I am new to this family, I would like to know about can configuration in detail. We are working on device using CAN protocol for communication, we would like to transmit and receive the CAN data from one device to another (SPC5). Based on the received data we would control the audio. 

Can anyone help us to how to enable, Initialize and configure the CAN protocol for SPC582Bxx family. 

This topic has been closed for replies.

14 replies

Rohit Rajapure
Associate III
Nov 21, 2023 5:04 AM UTC

Hi, 

Thanks for the quick response, 

I have followed the AVAS sample code (from tutorial), It worked as explained in tutorial. We want to work on similar project so chosen this sample for proceeding with implementation. 

Referred document - UM2719  AVAS architecture based on Auto Devkit. We have all setup as dev kit, audio kit and power kit. 

Dev kit - spc582b60e1 using. 

Sample code - SPC582Bxx_RLA_AEK_AUD_D903V1 - Engine Sound simulator with Connector board. 

Now, we are trying to test the CAN part of code, we have CAN transceiver and all setup but still not able to work. We are not getting whether the CAN section is enabled or not. 

We are new this, if you could guide us to test the same and as well as do the custom changes and linking of files (all library file to project) will help us to proceed further and work on this. 

 

Please share the file links steps as well as the enabling of CAN section and testing procedure for the same. 

 

Thanks and Regards

Rohit R

Associate
Nov 21, 2023 7:25 AM UTC

Hi,

i never use  Auto Devkit, bus if you want to use CAN-BUS try this example: 

SPC582Bxx_RLA_CAN Test Application

 

Rohit Rajapure
Associate III
Nov 23, 2023 5:54 AM UTC

Hi, 

As you suggested we are gone through the example but also in mean time we looked sample SPC582Bxx_RLA_AEK_AUD_D903V1 Engine_Sound_Simulator with Connector code,

Here, in Engine Sound Simulator code we saw the CAN transmit and Receive code snippet. But when we tried to execute the same we are unable to execute the CAN code. We tried to Receive the data but still not getting the result. 

Can you help me whether the CAN part is enabled in this code or not? If Not, then let us know how to enable the CAN section and even we are not able to find how to set baudrate or where the buad rate is been set?

Please help us to understand in detail about baud rate and other set regarding CAN. 

Thanks and Regards

Rohit R

Rohit Rajapure
Associate III
Nov 21, 2023 7:57 AM UTC

Hi, 

Thank you for the response,

Will check with sample and get back to you.

 

Thanks and Regards

Rohit R

Rohit Rajapure
Associate III
Nov 24, 2023 3:42 AM UTC

Hi,

Thanks for the response, 

CAN setting option is No_loopback, as you can see below, 

RohitRajapure_0-1700797050963.png

can you guide more detail about how to set this things if we want build the custom project?

Regarding the testing, we are using can analyzer to send some data, we are just checking the Rx part not transmitting part, 

We are verifying the below code section, 

void mcanconf_rxreceive(uint32_t msgbuf, CANRxFrame crfp)
{
(void)msgbuf;

if (crfp.ID == 0x7f0U)
{
if (crfp.data32[0] == 0xAABBCCDDUL) //START
{
state = START;
}
else
{
state = STOP;
}
}

}

Where is the baud rate set? we are unable to figure out the baud rate for this project. 

Please do share if any document which explain about setting up baud rate and other configuration It will help us to fast implementation. 

Waiting for positive response with complete guide. 

Thanks and Regards

Rohit R

Associate III
Nov 24, 2023 6:30 AM UTC

If you did not change anything from the example baud rate is 500. You selectvit with clock prescalar. I do not understand the clock setting myself bjt I found a way to switch between 250, 500 and 1000, a bit try and error I guess. 

Next thing: watch out for extended or standard frame. This is set up int the rx receive filter settings. Just double click the filter.

If you look here for my posts you can find a CAN thread which resolved some mysteries to me. Other than that I just went through the Application Note- you can find that also in the other thread. 

Associate III
Nov 24, 2023 6:34 AM UTC

Here is the application note you want to follow through with (Max post)

https://community.st.com/t5/autodevkit-ecosystem/autodevkit-2-2-can-examples-missing-version-bug/td-p/609030 

Rohit Rajapure
Associate III
Nov 27, 2023 10:59 AM UTC

Hi,

Did you checked my  previous post regarding the CAN analyzer and message error. 

I tried to follow the instructions and build the code from Strach we are getting the below error while configuring the CAN, let us know your feedback on this. 

RohitRajapure_0-1701082666980.png

Let me know how to make changes and enable them. And still I didn't get the baud rate configuration. 

And 500 baud rate is not working for the code. 

Please share the feedback for the issues. 

Thanks and Regards

Rohit R

Rohit Rajapure
Associate III
Nov 28, 2023 4:38 AM UTC

Hi, 

We are unable to figure out the configuration and test the CAN as you mentioned regarding the baud rate. 

Please share your feedback as early as possible.

 

Thanks and Regards,

Rohit R

Rohit Rajapure
Associate III
Nov 29, 2023 5:35 AM UTC

 Hello, 

Any feedback on my post. 

We need urgent help to fix this. 

Waiting for your response, 

 

Thanks and Regards

Rohit R