Skip to main content
kevin239955_st
Associate III
Oct 21, 2014 4:35 PM UTC
Question

SPC560B-DIS Discovery Board

Posted on October 21, 2014 at 18:35

Can't seem to connect to the SPC560B-DIS via USB or JTAG-USB (SOC5-UDESTK) to the UDE debugger. UDE does not list the device SPC560B54L5. UM1672 User Manual (Table 3) mentions some ''jumper'' states that are in actual fact not jumpers and would require soldering to change configuration.

Can someone help?

#spc5studio
    This topic has been closed for replies.

    12 replies

    souha
    Associate
    Jun 1, 2015 3:04 PM UTC
    Posted on June 01, 2015 at 17:04

    Hello,

    We are using the spc560B60L3 100 pin package in adevelopment project. We need to use 4 LINflex interfaces.

    In the data sheet, it is mentioned that it supports 4 LINs.Can we use LIN4 and LIN5 or it only supports LIN0 up to LIN3?

    Thanks

    Erwan YVIN
    ST Technical Moderator
    Jun 5, 2015 12:16 PM UTC
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.