Skip to main content
kevin239955_st
Associate III
Oct 21, 2014 4:35 PM UTC
Question

SPC560B-DIS Discovery Board

Posted on October 21, 2014 at 18:35

Can't seem to connect to the SPC560B-DIS via USB or JTAG-USB (SOC5-UDESTK) to the UDE debugger. UDE does not list the device SPC560B54L5. UM1672 User Manual (Table 3) mentions some ''jumper'' states that are in actual fact not jumpers and would require soldering to change configuration.

Can someone help?

#spc5studio
    This topic has been closed for replies.

    12 replies

    kevin239955_st
    Associate III
    Oct 23, 2014 12:02 PM UTC
    Posted on October 23, 2014 at 14:02

    Connection issue resolved (was IT related). Can anyone tell me where to find the software examples used in the Discovery kit tutorials? There is nothing at this link: 

    http://www.st.com/web/en/catalog/tools/PF259369

    .

    Erwan YVIN
    ST Technical Moderator
    Nov 14, 2014 1:39 PM UTC
    Posted on November 14, 2014 at 14:39

    Hello Kevin ,

    sorry for my late answer :

    we have some IT issues too ;)

    The software examples are present in the application wizard(2 at the current time for B Discovery)

    all the applications are uptodate in SPC5Studio 3.3

    (cf attachment)

    Best Regards

    Erwan

    ________________

    Attachments :

    2014-11-14_143607.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0UN&d=%2Fa%2F0X0000000bZc%2FLUjOeD5DRRiPoLM33C.rWuBjmTtwWdEJWKFkpVpcOD8&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    kevin239955_st
    Associate III
    Nov 26, 2014 5:09 PM UTC
    Posted on November 26, 2014 at 18:09

    Many thanks.

    kevin239955_st
    Associate III
    Jan 16, 2015 11:30 AM UTC
    Posted on January 16, 2015 at 12:30

    I am trying to connect to the Discovery board directly via JTAG (as opposed to the default, USB integrated debugger configuration). Table 3 of the reference manual (UM1672) says that a load of jumpers need changing if JTAG is to be used. However it looks as if these jumpers (J101, J102...) will require soldering, which is unexpected. Could you confirm this? I am currently unable to connect directly via JTAG (with either ST's UDESTK or a UAD2pro).

    Erwan YVIN
    ST Technical Moderator
    Jan 16, 2015 3:22 PM UTC
    Posted on January 16, 2015 at 16:22

    Hello Kevin ,

    No HW modification is required.

    Using the JTAG port only, the board must be supplied by using the external power supply.

    Note: J101 (0R resistor) in the default HW configuration must not be present.

       Best regards

                   Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ssk
    Associate III
    Jan 20, 2015 5:19 AM UTC
    Posted on January 20, 2015 at 06:19

    Hello Erwan,

    Can you please share the link for SPC5Studio 3.3 to download? ST Micro website displays v3.0 for download. Thanks.

    Mike.

    Erwan YVIN
    ST Technical Moderator
    Jan 20, 2015 8:33 AM UTC
    Posted on January 20, 2015 at 09:33

    Hello Mike ,

    You have to download SPC5Studio 3.0.

    and after , you can use the ''update site system'' from SPC5Studio

    ''Help ==> Install new Software''(Cf Screenshot)

    It will install SPC5Studio Core, Pinmap, Application Wizard 3.3.2.

    (cf Installation Details)

    Best regards

    Erwan

    ________________

    Attachments :

    2015-01-20_093226.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0SI&d=%2Fa%2F0X0000000bZb%2FWeKNFJypV_eqIysw7If3urW8iibZf4VuR7db44_oF_s&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ssk
    Associate III
    Jan 20, 2015 11:55 AM UTC
    Posted on January 20, 2015 at 12:55

    Thanks Erwan. It worked.

    Mike.

    kevin239955_st
    Associate III
    Jan 20, 2015 1:44 PM UTC
    Posted on January 20, 2015 at 14:44

    Erwan

    Thanks, after desoldering the probes now connect.

    Kevin

    Erwan YVIN
    ST Technical Moderator
    Jan 21, 2015 4:35 PM UTC
    Posted on January 21, 2015 at 17:35

    Good news ;)

        Best regards

            Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.