Skip to main content
TBran.3
Associate II
Jul 7, 2023 3:01 AM UTC
Solved

STM32WB FOTA Practical Questions

Hi all,

Looking to implement FOTA on a custom board which uses the STM32WB55M module. I understand the principles of the FOTA solution and the services/characteristics and have looked over the relevant app note, but I have a couple of questions about how precisely to actually implement the solution.

1. Would installing both the OTA application and the user application be a matter of compiling each (OTA app with a linker script specifying a start address of 0x08000000 and the user app at (IIRC) 0x08007000) separately and then loading each binary separately at the respective addresses?

2. For custom boards, is it typical to just use the OTA application given in the STM32CubeWB software package (with some slight modifications to, for example, the BSP functions which control Nucleo LEDs)?

In other words, what I *think* is the procedure, given that I currently have a custom board with a user application:

  1. Modify user app linker script to start at an address beyond where the OTA app will end
  2. Take the OTA app from STM32CubeWB and modify the HW-specific functions (i.e. LED controls) to match up with my hardware.
  3. Ensure VTOR is moved correctly for user application (at 0x08007000 instead of 0x08000000?)
  4. Add reboot request char to one of the services in my user application
  5. Compile both programs
  6. Load OTA app binary at 0x08000000 using CubeProg
  7. Load user app binary at 0x08007000 using CubeProg (or OTA)

Is that right or am I misunderstanding?

Thanks.

This topic has been closed for replies.
Jerry06Best answer
Visitor II
Oct 24, 2023 1:38 PM UTC

I experienced the same issue. Just mentioned in this post https://community.st.com/t5/stm32-mcus-wireless/stm32wb-cpu1-stuck-waiting-cpu2-at-init/m-p/580103#M16082, the problem is caused by that, the clock of the application is configured on the HSE and the bootloader is on LSE for the RF system wakeup. So configuring the clock source of RF system wakeup to LSE in your application is a way to solve the problem.

19 replies

Visitor II
Jul 11, 2023 9:44 AM UTC

Hi, 

I have the same issue and I think like you but i'm not sure it is correct.

TBran.3
TBran.3Author
Associate II
Jul 12, 2023 3:04 AM UTC

I should note that it appears the default OTA app already handles VTOR correctly, shouldn't require any changes there, other than to comment out the VTOR update in the user application startup code.

I followed my proposed process above and it appears that the application never boots though, so still some debugging to do. It seems too that this *should* be the process based on the notes in the readme.txt found in the BLE_p2pServer_ota example in STM32CubeWB.

TBran.3
TBran.3Author
Associate II
Jul 12, 2023 4:24 AM UTC

Ok it looks like it just needed a power cycle. After following more or less the above process, I can write to the reboot request char and get the app to reboot into the OTA app. I can even debug the OTA app and catch the point at which it jumps into it after the reboot request, but it never seems to advertise as STM_OTA. The OTA app and not the user app is clearly running though. What am I missing?

Associate III
Aug 24, 2023 8:26 AM UTC

I have the exact same problem. Not advertising as STM_OTA but also my user code is not deleted, is that also the case for you?

TBran.3
TBran.3Author
Associate II
Aug 24, 2023 7:19 PM UTC

Yep. I can power cycle to boot back into the user app IIRC. It's like it's waiting for CPU2 to reset or reinit or something, but the strange thing is that if I send 0x00 (App reboot) instead of 0x01 0x07 0xFF (FOTA reboot), it jumps to the OTA bootloader and back into my user app just fine. 

To answer your question about the while(1), you're right, the code should never get there, just added it while experimenting with stuff. Not really needed.

I'm pulling my hair out with this. I'm just hoping someone from ST can reply with an answer at this point. It seems at least 3 or 4 of us on this forum have had this problem in the last month or so.

TBran.3
TBran.3Author
Associate II
Jul 15, 2023 2:29 PM UTC

So when I issue the reboot command and it jumps into the OTA app, it seems to hang here. It's just idling waiting for an event it appears, so it never exits SHCI_C2_BLE_Init(), which means it never makes it to Ble_Hci_Gap_Gatt_Init(). Is this a bug in the OTA app or does this mean I haven't commanded the reset correctly somehow?

TBran3_0-1689431073020.png

 

TBran.3
TBran.3Author
Associate II
Jul 29, 2023 3:34 AM UTC

I'm still stuck here. Tried a few things but have never been able to track down the issue. Anyone out there ever run into this or have any ideas?

OliM
Senior II
Aug 7, 2023 11:06 AM UTC

What is missing from your description and probably also from your code is the magic number used by the OTA application to verify that you have a good Firmware.

OliM_0-1691406351756.png

OliM_1-1691406376383.png

 

 

TBran.3
TBran.3Author
Associate II
Aug 8, 2023 3:12 AM UTC

I have these, as long as I didn't make a typo somewhere.

C definitions, in app_ble.c:

TBran3_0-1691464152840.png

Linker file changes:

TBran3_1-1691464187002.png

TBran3_2-1691464206232.png

TBran3_3-1691464225826.png

I'm attaching my entire linker file...

 

TBran.3
TBran.3Author
Associate II
Aug 8, 2023 3:25 AM UTC

While I'm at it, here's the relevant sections from other parts of the code as well:
custom_stm.c, handling the incoming reboot request:

TBran3_2-1691465006695.png

 

 

custom_app.c, actually processing the reboot request:

 

TBran3_3-1691465013139.png

Interestingly enough, if I write a 0 to the reboot request characteristic, which corresponds to a request to reboot into the user application, that works correctly. It is only when I send 0x01 0x07 0x<num sectors> to enter OTA update mode that the OTA loader application hangs.

Associate III
Aug 24, 2023 8:30 AM UTC

Why do you have a while(1) after the SystemReset? That's never going to be executed, right?

Associate III
Sep 14, 2023 7:00 AM UTC

Any progress on this? I just gave up, as it was just wasting time..