Skip to main content
Associate III
Aug 7, 2023 10:53 AM UTC
Solved

TouchGFX Circle progress very limited configurability

Using TouchGFX Designer 4.22.0

Why it is not possible to make a circle progress much like a car dashboard would have. Zero is at about 7 o'clock and full is at 4 o'clock.

The circle progress always starts at 12:00. No mater what parameters I enter.

Is there another method of achieving similar effect?

    This topic has been closed for replies.
    JTP1Best answer
    Graduate II
    Aug 7, 2023 2:11 PM UTC

    Hello

    I test it quicky and yes, the designer shows it completely wrong in the new versions.

    However, it seems to work on the simulator and target. Have you test to run it ?

    Br J.T

    6 replies

    tarmogrAuthor
    Associate III
    Aug 7, 2023 11:23 AM UTC

    Just downloaded v4.18. Although the design there is a little different(even more options???) this one seems to be working. Adjusting the "Start" angle actually changes the start position. So it seems that 4.22 has a bug.

    Oh why always after having so much work to get it to work you discover some bug that makes it unusable :face_with_tears_of_joy:

    See comparsion images attached.

    tarmogrAuthor
    Associate III
    Aug 7, 2023 12:01 PM UTC

    Ok did some more tests with 4.21.4. This one also has the same bug. Am I missing something? How have people used this widget in past? Could it be corrected in STMCube?

    JTP1Best answer
    Graduate II
    Aug 7, 2023 2:11 PM UTC

    Hello

    I test it quicky and yes, the designer shows it completely wrong in the new versions.

    However, it seems to work on the simulator and target. Have you test to run it ?

    Br J.T

    tarmogrAuthor
    Associate III
    Aug 7, 2023 8:22 PM UTC

    I had a chance to test it on target. Yes indeed it seems to be running OK here, I hae not fully tested it but seems to be working now.

    Thanks

    Graduate II
    Aug 8, 2023 4:02 AM UTC

    Hello

    Good . It is still definitely a bug since its showed completely wrong in Tgfx designer which makes setting the parameters difficult and confuses users. 

    Br J.T

    Osman SOYKURT
    ST Technical Moderator
    Aug 21, 2023 2:40 PM UTC

    Hello @tarmogr and @JTP1 ,

    Thank you for reporting this issue. We will investigate on it, I'll keep you updated.

    ST Software Developer | TouchGFX