Skip to main content
awiernie
Associate III
Jun 21, 2023 12:02 PM UTC
Question

Touchgfx designer 4.22 crashes

After upgrading from TouchGFX 4.21.3 to Touchfx 4.22.0 the project was converted. If I open the touchgfx project the touchgfx designer crashes:

 

Application: TouchGFXDesigner-4.22.0.exe
CoreCLR Version: 7.0.122.56804
.NET Version: 7.0.1
Description: The process was terminated due to an unhandled exception.
Exception Info: System.IndexOutOfRangeException: Index was outside the bounds of the array.
at TouchGFXDesigner.Communications.NewsManagerViewModel.SwitchCurrentCard(Object state)
at System.Threading.ExecutionContext.RunInternal(ExecutionContext executionContext, ContextCallback callback, Object state)
--- End of stack trace from previous location ---
at System.Threading.ExecutionContext.RunInternal(ExecutionContext executionContext, ContextCallback callback, Object state)
at System.Threading.TimerQueueTimer.Fire(Boolean isThreadPool)
at System.Threading.TimerQueue.FireNextTimers()
at System.Threading.ThreadPoolWorkQueue.Dispatch()
at System.Threading.PortableThreadPool.WorkerThread.WorkerThreadStart()

    This topic has been closed for replies.

    3 replies

    Osman SOYKURT
    ST Technical Moderator
    Jun 21, 2023 12:39 PM UTC

    Hello @awiernie 

    Could you share with us your 4.21.3 project? We would need it to investigate what's happening here.
    (You can share it to me in PM if you prefer).

    ST Software Developer | TouchGFX
    awiernie
    awiernieAuthor
    Associate III
    Jun 21, 2023 1:24 PM UTC

    I have sent you a download link for the whole STM32CubeIDE project. 

    awiernie
    awiernieAuthor
    Associate III
    Jun 21, 2023 12:47 PM UTC

    It occures a few seconds after loading (without any user interaction) or after a few minutes with the same windows event log.