cancel
Showing results for 
Search instead for 
Did you mean: 

what does the line 6 wait do?

David.Cheng
Associate II
void sEE_ReadBuffer(uint8_t* pBuffer, uint16_t ReadAddr, uint16_t* NumByteToRead)
{
  //__IO uint32_t timeout = 0xFFFF;
  __IO uint32_t timeout = 0xf00;
  /*!< Wait the end of last communication */
  for (;timeout > 0; timeout--);
 
  /* Set the pointer to the Number of data to be read. This pointer will be used
      by the DMA Transfer Complete interrupt Handler in order to reset the 
      variable to 0. User should check on this variable in order to know if the 
      DMA transfer has been completed or not. */
  sEEDataReadPointer = NumByteToRead;
 
  /*!< While the bus is busy */
  while (I2C_GetFlagStatus(sEE_I2C, I2C_FLAG_BUSY))
  {}
 
  /*!< Send START condition */
  I2C_GenerateSTART(sEE_I2C, ENABLE);
 
  /*!< Test on EV5 and clear it */
  while (!I2C_CheckEvent(sEE_I2C, I2C_EVENT_MASTER_MODE_SELECT))
  {}
 
 
}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

What code is this? On which STM32?

As the comment says, it's a wait between "packets". There's no delay mechanism between STOP and subsequent START at least in some of the I2C modules, so back to back "packets" are confusing some slaves.

Loopdelay is nasty but simple.

JW

example code from st. STM8L152