Skip to main content
KDesr.1
Associate III
September 21, 2020
Question

STM8S ADC Scan Mode not updating

  • September 21, 2020
  • 0 replies
  • 1269 views

I am able to read my two ADC inputs individually when I implement the code shown in this example: http://embedded-lab.com/blog/starting-stm8-microcontrollers/13/

However, the ADC values in the buffers do not seem to be getting updated when I try to get the ADC to work in multi-input mode as per the example here: http://embedded-lab.com/blog/continuing-stm8-microcontroller-expedition/2/

I've looked at different locations in the ADC1_GetBufferValue() buffer, and none of them seem to be getting updated.

Perhaps I have modified something incorrectly for my application?

Here is my code, the specific device is the STM8S003F3.

#include "STM8S.h"

#include "STM8S_DELAY.h"

#include "MY_UART.h"

void Clock_Setup(void);

void GPIO_Setup(void);

void UART1_Setup(void);

void ADC1_Setup(void);

void TIM2_Setup(void);

void main (void)

{

char short_adc = 0x00;

char batt_adc = 0x00;

char tx_buffer[16];

int short_count = 0;

int i = 0;

// configure peripherals

  GPIO_Setup();

Clock_Setup();

ADC1_Setup();

  UART1_Setup();

while(1)

{

  ADC1_ScanModeCmd(ENABLE);

    ADC1_StartConversion();

    while(ADC1_GetFlagStatus(ADC1_FLAG_EOC) == FALSE);

    ADC1_ClearFlag(ADC1_FLAG_EOC); //clear the ADC conversion flag

  batt_adc = ADC1_GetBufferValue(2) >> 2; //update the ADC value

  short_adc = ADC1_GetBufferValue(3) >> 2;

  //Transmit the ADC value to the terminal

  my_itoa(batt_adc, tx_buffer); //convert the int to a string

  UART_SendStr("ADC value: ");

  UART_SendStr(tx_buffer);

  UART_SendChar(10); //LF

  UART_SendChar(13); //CR

}

}

void Clock_Setup(void)

{

CLK_DeInit();

CLK_HSECmd(DISABLE);

CLK_LSICmd(DISABLE);

CLK_HSICmd(ENABLE);

while(CLK_GetFlagStatus(CLK_FLAG_HSIRDY) == FALSE);

CLK_ClockSwitchCmd(ENABLE);

CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);

CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);

CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSI, 

DISABLE, CLK_CURRENTCLOCKSTATE_ENABLE);

CLK_PeripheralClockConfig(CLK_PERIPHERAL_I2C, DISABLE);

CLK_PeripheralClockConfig(CLK_PERIPHERAL_SPI, DISABLE);

CLK_PeripheralClockConfig(CLK_PERIPHERAL_ADC, ENABLE);

CLK_PeripheralClockConfig(CLK_PERIPHERAL_AWU, DISABLE);

CLK_PeripheralClockConfig(CLK_PERIPHERAL_UART1, ENABLE);

CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER1, DISABLE);

CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, ENABLE);

CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER4, DISABLE);

}

void GPIO_Setup(void)

{

// PC3 - Input

// PC4 - VBatt - ADC AIN2)

// PD2 - Short - ADC AIN3)

// PD3 - Low Batt LED

// PD4 - Strobe LED

// PD5 - UART1 TX

// PD6 - UART1 RX

GPIO_DeInit(GPIOC);

GPIO_Init(GPIOC, GPIO_PIN_3, GPIO_MODE_IN_PU_IT);

GPIO_Init(GPIOC, GPIO_PIN_4, GPIO_MODE_IN_FL_NO_IT);

  GPIO_DeInit(GPIOD);

GPIO_Init(GPIOD, GPIO_PIN_2, GPIO_MODE_IN_FL_NO_IT);

GPIO_Init(GPIOD, GPIO_PIN_3, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(GPIOD, GPIO_PIN_4, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_OUT_PP_LOW_FAST);

GPIO_Init(GPIOD, GPIO_PIN_6, GPIO_MODE_IN_PU_NO_IT);

}

void UART1_Setup(void)

{

 UART1_DeInit();

  UART1_Init(9600, 

        UART1_WORDLENGTH_8D, 

        UART1_STOPBITS_1, 

        UART1_PARITY_NO, 

        UART1_SYNCMODE_CLOCK_DISABLE, 

        UART1_MODE_TXRX_ENABLE);

  UART1_Cmd(ENABLE);

}

void ADC1_Setup(void)

{

ADC1_DeInit();     

 ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, 

       ADC1_CHANNEL_2,

       ADC1_PRESSEL_FCPU_D18,

       ADC1_EXTTRIG_GPIO,

       DISABLE,

       ADC1_ALIGN_RIGHT,

       ADC1_SCHMITTTRIG_CHANNEL2,

       DISABLE);

  ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, 

       ADC1_CHANNEL_3,

       ADC1_PRESSEL_FCPU_D18,

       ADC1_EXTTRIG_GPIO,

       DISABLE,

      ADC1_ALIGN_RIGHT,

       ADC1_SCHMITTTRIG_CHANNEL3,

       DISABLE);

  ADC1_ConversionConfig(ADC1_CONVERSIONMODE_CONTINUOUS,

            ((ADC1_Channel_TypeDef)(ADC1_CHANNEL_2 | ADC1_CHANNEL_3)),

ADC1_ALIGN_RIGHT);

  ADC1_DataBufferCmd(ENABLE);

  ADC1_Cmd(ENABLE);

}

    This topic has been closed for replies.