Skip to main content
PPate.1
Associate III
September 15, 2020
Question

STM8A wakeup from HALT by CAN Rx interrupt not working

  • September 15, 2020
  • 0 replies
  • 908 views

I am using STM8AF5286 controller and CAN port for external communication. My application need to be in HALT mode to prevent battery consumption and wakeup only when any activity is detected on CAN port. The application works fine with wfi() function but it does not wakeup if I use halt().

I am using STM8 standard peripheral library.

CAN is configured as below:

/* CAN RX pin interface */

GPIO_DeInit(GPIOG);

GPIO_Init(GPIOG, GPIO_PIN_1, GPIO_MODE_IN_PU_IT);

/* CAN register init */

 CAN_DeInit();

 /* CAN init */

 CAN_MasterCtrl=CAN_MasterCtrl_AllDisabled;

 CAN_Mode = CAN_Mode_Normal;

 CAN_SynJumpWidth = CAN_SynJumpWidth_1TimeQuantum;

 CAN_BitSeg1 = CAN_BitSeg1_8TimeQuantum;

 CAN_BitSeg2 = CAN_BitSeg2_7TimeQuantum;

 CAN_Prescaler = 4; //set to 250Kbps, set to 2 for 500Kbps

 status = CAN_Init(CAN_MasterCtrl, CAN_Mode, CAN_SynJumpWidth, CAN_BitSeg1, \

          CAN_BitSeg2, CAN_Prescaler);

CAN_ITConfig(CAN_IT_WKU, ENABLE);

My application code :

while(1){

----

state machine

----

case wait_mode:

CAN_Sleep();

halt();

break;

}

In CAN Rx interrupt handler I toggled GPIO which is not responded even if receive message on CAN port after entering in halt().

    This topic has been closed for replies.