cancel
Showing results for 
Search instead for 
Did you mean: 

how to use 64 bit data type in stm8s003

agilandeswari
Associate
Posted on September 07, 2015 at 12:00

how to use 64 bit data type in stm8s003f3? if i use unsigned long long its not takeing and giving error.

#st
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
luca239955_stm1_st
Senior II
Posted on September 07, 2015 at 12:22

which compiler?

If it's Cosmic, the long long (64 bits) datatype is not implemented for the STM8, since it would be very heavy for such a small core to handle such a large datatype.

Regards.

Philipp Krause
Senior III
Posted on September 09, 2015 at 19:03

64-bit integers were introduced in the ISO C99 standard, which, as far as I know, is supported by SDCC and IAR C, but not the other compilers.

In C99 on STM8 you can use long long, unsigned long long, uint16_t int64_t, uint_fast64_t, uint_least64_t, int_fast64_t, int_least64_t.

Philipp