Solved
STM32G0 unable to connect via SWD
I tried to connect the STLink to the STM32G030K6T6 by connecting SWCLK SWDIO VDD and GND pins, but the STM32CubeProgrammer can't detect the MCU.
I also tried to check with the logic analizer the pins and there is only a little signal from the stlink but no response from the MCU.
I think the problem could be that the SWCLK and BOOT0 are in the same pin and this is pulled down internally. So how can I connect and program the STM32?
Thank you so much