Skip to main content
Associate II
February 19, 2026
Question

STM32CubeProgrammer Verification Error with External QSPI Loader

  • February 19, 2026
  • 1 reply
  • 316 views

When using a STM32H757, with external QSPI, on an STM32H757I-EVAL, I am experiencing some programming issues when programming an .elf file with sections pointing to external QSPI. I am using the ST External Loader for MT25TL01G_STM32H747I-EVAL. Programming does work successfully, but on newer versions of cube programmer, there are warnings about 32 byte alignment, and then verification fails.

 

The addresses mentioned are in AXI SRAM, and are .bss sections, which are marked NOLOAD, so it's confusing why that memory is trying to be programmed and this error is coming up in the first place. Manually setting the ALIGN markers in the linker file to be 32 instead of 4 does seem to get rid of the warning, and fix the issue.

 

I've seen this issue on with versions 2.19 and 2.21 Is this a known issue?

 

I haven't seen this issue with 2.17.

 

Attached are logs files with the warnings and errors. Thanks for the help!

1 reply

Aziz BRIGUI
ST Technical Moderator
February 24, 2026

Hi @eng88,

Could you dump the program headers for your elf file here please?

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
eng88Author
Associate II
February 24, 2026

Yes, I've attached it to the original question. Thanks!

Aziz BRIGUI
ST Technical Moderator
February 25, 2026

Hi @eng88,

I see that AXI SRAM segments are load segments:AXISRAM_loadSegments.png

Could you set them to NO_LOAD and retry ?

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.