Skip to main content
Associate II
Apr 11, 2024 7:28 AM UTC
Question

STM32CubeProgrammer on Ubuntu: DisplayResolution

Dear All,

 

Hi, I am using STM32CubeProgrammer in Ubuntu system, but the resolution is not right. Could you please help me fix the problem? Thank you so much!

Screenshot from 2024-04-11 03-22-50.png

Best

This topic has been closed for replies.

12 replies

Uwe Bonnes
Chief
Apr 11, 2024 10:14 AM UTC

The messages are in the picture are too small to be readable, So we can not help you to interpret these messages.

Gerald_WAuthor
Associate II
Apr 12, 2024 7:17 PM UTC

Dear Bonnes,

Thank you for your reply. In fact, the font being too small is exactly the problem, I can't increase it anyway.

Best

Andrew Neil
Super User
Apr 11, 2024 10:29 AM UTC

@Gerald_W wrote:

the resolution is not right.


What do you mean by that?

That the text is too small?

Is the CubeIDE similarly affected?

And other apps?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Gerald_WAuthor
Associate II
Apr 12, 2024 7:21 PM UTC

Dear Mr. Neil,

Thanks for your replying. Because my computer screen resolution is high. But STM32CubeProgrammer cannot adapt to high resolution, the text is too small. STM32CubeIDE works well and displays very clearly like other software with system font size.

 

Best

Uwe Bonnes
Chief
Apr 15, 2024 11:18 AM UTC

Did you start the program from the command line? Did it spew out messages there? Start from the command lien and check for missing fonts.

Andrew Neil
Super User
Apr 18, 2024 8:44 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Visitor II
Jun 13, 2025 4:16 AM UTC

lduquef_0-1749788106234.png

This changes work for Me , Preferences->STM32Cube->Divece Configuration Tool->display size-> Large.

Associate II
Jun 13, 2025 10:04 AM UTC

Thanks for trying to help. The above is for STM32CubeMX. This program has an option to increase the size of the text. The STM32CubeProgrammer has no option.