Skip to main content
Ah.1
Associate
Jan 30, 2020 1:53 PM UTC
Solved

Installing STM32CubeProgrammer on Raspberry Pi

We've been succesfully using stm32flash in the past to flash our STM32 MCU that are attached to Raspberry Pi servers (no desktop or X). As we moved on to STM32G0 it seems that stm32flash is no longer working and we are forced to use STM32CubeProg to flash our firmware.

Is it possible to install STM32CubeProg on a) ARM such as RPI, b) server with no desktop?

To begin with, the installation instructions require the installation of OpenJFX which is not relevant (nor possible, in lieu of X) in this case, we intend to use only the CLI interface through scripts that perform the flashing.

Then, trying to run the installation script on the RPI fails since the provided installation binary is for x86.

Houda GHABRI
Houda GHABRIBest answer
ST Employee
Jun 16, 2020 12:52 PM UTC

Hi ,

It is not possible for the moment to install STM32CubeProgrammer on ARM processor.

There is plan to do it but unfortunately not in the near future.

regards,

Houda

41 replies

olivier
Associate
Feb 4, 2020 8:35 AM UTC

Hi,

I would also definitely like to see an ARM version of STM32CubeProgrammer (at least the CLI) that would run on Raspberry Pi (and STM32MP1).

@Khouloud GARSI​ @Nawres GHARBI​ is this something we can hope for in the near future?

Thanks

Olivier

AMiro.2
Visitor II
Jun 2, 2020 6:39 AM UTC

This is needed for me as well

TJaku.1
Associate
Jun 10, 2020 6:51 AM UTC

We would also like to use STM32_Programmer_CLI on Raspberry Pi.

KChud.1
Associate
Jun 16, 2020 10:01 AM UTC

HI,

I need in my some projects raspberry pi needs to program the stm32, so please provide some help for this.

CLI version is sufficient , please help me in this.

Houda GHABRI
Houda GHABRIBest answer
ST Employee
Jun 16, 2020 12:52 PM UTC

Hi ,

It is not possible for the moment to install STM32CubeProgrammer on ARM processor.

There is plan to do it but unfortunately not in the near future.

regards,

Houda

KChud.1
Associate
Jun 16, 2020 12:58 PM UTC

Thank you for prompt response.

Is there any other way or any cli file that I installed in raspberry and make this done?

Associate III
Jan 1, 2026 10:42 AM UTC

the possible way to write a bootloader and flash it initial memory of flash. In that enumerate I2C and connect I2C cables. Also write flash operation using i2c So through i2c you can do binary flashing to your MCU

AMiro.2
Visitor II
Jun 16, 2020 1:56 PM UTC

Try openocd. It works for me well.​

Associate
Dec 29, 2025 2:38 PM UTC

Got it to work with stlink-tools and st-flash

Andrew Neil
Super User
Dec 30, 2025 11:30 AM UTC

@fghoussen wrote:

Got it to work with stlink-tools and st-flash


For the benefit of other readers, can you give more details of that?

Are these the tools:

https://packages.debian.org/sid/electronics/stlink-tools

https://man.archlinux.org/man/extra/stlink/st-flash.1.en

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Rstua.1
Senior
Mar 3, 2021 8:08 PM UTC

 ...

Rstua.1
Senior
Mar 3, 2021 8:20 PM UTC

Has anyone successfully run STM32_Programmer_CLI on the Raspberry Pi using QEMU? I think you will also have to run the USB drivers from STMicro. Which makes this all the more obfuscated.

PADAM.1
Associate III
Mar 4, 2021 11:54 AM UTC

As stated by Houda Ghabri (ST Employee) above, there were no plans to port CubeProgrammer on Rasperry Pi.

To my opinion, from customer point of view this position is an error and should evolve.

OpenOCD is only a work around and I think it cannot support SBSFU (may be I am wrong and someone has done?)

Thus let's continue to ask...

Rstua.1
Senior
Mar 4, 2021 1:35 PM UTC

I had a sales rep recently infer after talking to STMicro that there is still a though that STMicro would port STM32_Programmer_CLI to and ARM type processor. I am interested in field upgrades using a Raspberry Pi. But can see a more general much more robust need for field upgrade tools running on an ARM processor if ARM based Android COTS computers and small form factor ARM based computers were included in the mix.

As it stands, no STMicro support for ARM based STM32 programming tools, we are considering writing our own boot loader and abandoning the STMicro's boot loader & USB driver (as I assume the STMicro USB driver just makes the over all upgrading process more obfuscated).

RMora.4
Associate III
Aug 7, 2021 2:57 PM UTC

How is the progress on this? Can I use the command line tool in STM32CubeProgrammer to flash an STM32 from a raspberry pi? If that's not possible what is the work around? Is there another utility that I can use? ST-LINK utility maybe? does this tool work on ARM? How about one of JLinks software like JFlash? Which I know definitely runs on ARM.

I noted a comment about openocd - I'll give this a shot.