Skip to main content
Associate II
May 14, 2026
Solved

cube programmer shows 256 pages of 2K in a 256K mcu?

I am using a stm32 F103RCT6 mcu. It has 256 Kb of flash memory. But when i connect it to cube programmer, it shows there are 256 sectors of 2K size which equates to 512 Kb flash. 

I was even able to go to that last page and write data to it. so is the linker script generated by HAL wrong?

Akshat_codes__0-1778745508180.png

Akshat_codes__1-1778745517616.png

 

 

AScha.3
AScha.3Best answer
Super User
May 14, 2026

Nothing wrong here. :)

Just you got a F103 with full flash, 512K.  

Reason is: for the purpose of rationalized production only one die is produced , with 512K .

Testing the flash is "expensive" on the chip tester, so short test -> smaller flash tested -> cheaper version.

So you have a chip with 256K flash, tested and 100% working - as you ordered.

And there is more flash on the die, might work fine or not - you didnt pay for tested 512K .

So you can use it, but dont cry, if there is an error....

And linker script is ok, if 256K is used, as you ordered.

If you feel a post has answered your question, please click on " Best Answer ".

7 replies

Andrew Neil
Super User
May 14, 2026

@Akshat_codes_ wrote:

I am using a stm32 F103RCT6


Where did you obtain it?

Are you sure it is genuine?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
May 14, 2026

I ordered it from LCSC. Attached below is the image

Akshat_codes__0-1778746305694.jpeg

 

Andrew Neil
Super User
May 14, 2026

@Akshat_codes_ wrote:

I ordered it from LCSC.


You mean here: https://www.lcsc.com/ ?

Not an Authorised Distributor, so there is a risk it's fake.

 

Maybe this diagnostic can help you identify it ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AScha.3
AScha.3Best answer
Super User
May 14, 2026

Nothing wrong here. :)

Just you got a F103 with full flash, 512K.  

Reason is: for the purpose of rationalized production only one die is produced , with 512K .

Testing the flash is "expensive" on the chip tester, so short test -> smaller flash tested -> cheaper version.

So you have a chip with 256K flash, tested and 100% working - as you ordered.

And there is more flash on the die, might work fine or not - you didnt pay for tested 512K .

So you can use it, but dont cry, if there is an error....

And linker script is ok, if 256K is used, as you ordered.

If you feel a post has answered your question, please click on " Best Answer ".
Andrew Neil
Super User
May 14, 2026

but shouldn't CubeIDE CubeProgrammer recognise the chip from its ID, and only report the specified memory sizes ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AScha.3
Super User
May 14, 2026

Maybe, if different ID is written to chip, but basically is same die for c-d-e flash size:

AScha3_0-1778747908824.png

vs.

connect a H743ZG  , 1MB flash (but die has 2MB :(

AScha3_1-1778748371625.png

and all are 450 die :

AScha3_2-1778748505504.png

But obviously here something written to the chip, to disable dual core, flash size info, etc.

So i tried using the 2MB flash - and yes, its there - but not tested, as ordered version has 1MB.

+ here connect to H743ZI , 2MB  , ordered:

AScha3_3-1778748900259.png

2MB verified.

If you feel a post has answered your question, please click on " Best Answer ".
Associate II
May 14, 2026

ok thanks for the response.