Skip to main content
Associate
Aug 28, 2024 8:36 AM UTC
Question

Can not connect to Board in with DFU Mode, only after initialize connection with ST-LINK

Hello 

I've problems connecting via DFU. The cubeprogrammer is trying, but never reaches the connected state. 

However, if I connect one time with a ST-Link device, the disconnect and switch to DFU then it works as long I do not close the CubeProgrammer instance. 

 

Does anyone know why this is the case and what I can do to connect on the first try?

 

The first screenshot is when the conneciton does not work

ConnectionFailure.png

Second is from a successfull connection

ConnectionSuccess.png

 

 

This topic has been closed for replies.

3 replies

mƎALLEm
ST Technical Moderator
Aug 28, 2024 8:40 AM UTC

Hello @egse112 and welcome to the community.

You need to provide which MCU part number and which board are you using.

How are you doing the procedure to connect in DFU mode with cube programmer including the HW manipulation: BOOT pin and RESET.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
egse112Author
Associate
Aug 28, 2024 9:03 AM UTC

Hi SofLit, 

Here you are:

targetinfo.png

I am connecting in DFU mode by selecting the Device in the Programmer and click on connect. 

connectionIfno.png

 

 

mƎALLEm
ST Technical Moderator
Aug 28, 2024 9:21 AM UTC

Ok but how you did handle BOOT pin and reset?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.