Skip to main content
yves2brest
Associate II
March 1, 2022
Question

When I see in STM32CubeMX the X-CUBE-TOF1 package if I try to load it. He answers me this package is already there. , I don’t see it appearing under Middleware as in the user manual , UM2978

  • March 1, 2022
  • 3 replies
  • 1121 views

..

This topic has been closed for replies.

3 replies

Sara BEN HADJ YAHYA
ST Technical Moderator
March 2, 2022

Hello @yves2brest​ ,

Thanks for your feedback,

I am not sure I understood correctly your request, could you please share a detailed scenario, or a capture describing your issue?

Thanks,

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
yves2brest
Associate II
March 17, 2022
Hello Sara, Excuse me, for not having answered you immediately, but to your message I understood that it was necessary to use CubeMX in Stm32CubeIde18 instead of CubeMX alone. Then the program did not work because there was a missing Callback function. in the main.c on the interrupt caused by the VL53L1 sensor on the X-NUCLEO-53L1A1 expansion board. I introduced this piece of code into the code generated by Stm32CubeIde18 but does not work. I think I have to ask another question and a TOF specialist will answer. in app_tof.c. I want introduce : RANGING_SENSOR_ROIConfig_t roiConfig; roiConfig.TopLeftX=12; roiConfig.TopLeftY=12; roiConfig.BotRightX=4; roiConfig.BotRightY=4; status = VL53L1A2_RANGING_SENSOR_ConfigROI(VL53L1A2_DEV_CENTER,&roiConfig ); tempstatus=status; if (status != BSP_ERROR_NONE) { printf("VL53L1A2_RANGING_SENSOR_Start failed ROI\n"); printf("status =%E\n, status"); while(1); Could you send me the name of a TOF specialist? Best regards Yves Mevel <> Garanti sans virus. www.avg.com <> <#DAB4FAD8-2DD7-40BB-A1B8-4E2AA1F9FDF2>
CLUGA.1
Visitor II
June 16, 2022

Hello @yves2brest,

I read you didn't find the interrupt callback, it is coded within the file app_tof_pin_conf.c but I understood you found a way to fix it by yourself.

Regarding the ROI the definition of the region of interest is a bit tricky.

0693W00000Ns1nsQAB.pngTo match your needs you should set 

 roiConfig.TopLeftX=4;

 roiConfig.TopLeftY=12;

 roiConfig.BotRightX=12;

 roiConfig.BotRightY=4;

Best Regards,

Christophe Lugand