Skip to main content
LucaP
Associate II
March 2, 2025
Solved

USB HS clocks not started from CubeMX 6.13 onwards

I am using the STM32F723 with custom, self-powered PCB interfaced to a host using USB HS. Everything worked fine with with CubeMX 6.12, but after upgrading to more recent versions, I noticed that the following functions are no longer generated within HAL_PCD_MspInit() (file usbd_conf.c):    

 

__HAL_RCC_USB_OTG_HS_CLK_ENABLE();
__HAL_RCC_USB_OTG_HS_ULPI_CLK_ENABLE();
 
and also the corresponding clock-disabling functions in HAL_PCD_MspDeInit(). If I manually re-insert these calls, everything works again.
Anyone knows the reason why these functions are not generated, and if I am missing any USB_HS setting in more recent CubeMX versions that should be taking care of this issue? Thanks!
This topic has been closed for replies.
FBLBest answer
ST Technical Moderator
March 7, 2025

Hi @LucaP 

Thank you for reporting and reproducing with latest version.

The issue is reported to dedicated team for a fix in code generation. Ticket number 204861 for reference.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

7 replies

TDK
March 3, 2025

Include the IOC that you think is generating faulty code.

"If you feel a post has answered your question, please click ""Accept as Solution""."
LucaP
LucaPAuthor
Associate II
March 7, 2025

Sorry for missing your request....attached are IOC projects created from scratch with CubeMX 6.12 and 6.14 respectively, based on the same MCU with only a HS USB and CDC activated. As you can see, usbd_conf.c generated by 6.12 calls the functions above, while the 6.14 does not.

From CubeMX 6.12:

 

 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**USB_OTG_HS GPIO Configuration
 PB13 ------> USB_OTG_HS_VBUS
 PB14 ------> USB_OTG_HS_DM
 PB15 ------> USB_OTG_HS_DP
 */
 GPIO_InitStruct.Pin = GPIO_PIN_13;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = GPIO_PIN_14|GPIO_PIN_15;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF12_OTG_HS_FS;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /* Peripheral clock enable */
 __HAL_RCC_OTGPHYC_CLK_ENABLE();
 __HAL_RCC_USB_OTG_HS_CLK_ENABLE();
 __HAL_RCC_USB_OTG_HS_ULPI_CLK_ENABLE();

 /* Peripheral interrupt init */
 HAL_NVIC_SetPriority(OTG_HS_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(OTG_HS_IRQn);

 

  vs. 6.14

 

 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**USB_OTG_HS GPIO Configuration
 PB13 ------> USB_OTG_HS_VBUS
 PB14 ------> USB_OTG_HS_DM
 PB15 ------> USB_OTG_HS_DP
 */
 GPIO_InitStruct.Pin = GPIO_PIN_13;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = GPIO_PIN_14|GPIO_PIN_15;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF12_OTG_HS_FS;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /* Peripheral clock enable */
 __HAL_RCC_OTGPHYC_CLK_ENABLE();

 /* Peripheral interrupt init */
 HAL_NVIC_SetPriority(OTG_HS_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(OTG_HS_IRQn);

 

 

ST Technical Moderator
March 3, 2025

Hi @LucaP 

Try to reproduce with latest version V6.14 first.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
LucaP
LucaPAuthor
Associate II
March 7, 2025

Done, please see reply to @TDK above.

FBLBest answer
ST Technical Moderator
March 7, 2025

Hi @LucaP 

Thank you for reporting and reproducing with latest version.

The issue is reported to dedicated team for a fix in code generation. Ticket number 204861 for reference.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
LucaP
LucaPAuthor
Associate II
March 12, 2025

Thank you, @FBL 

In these cases, would a fix be typically released in a major release like CubeMX 6.15, or a minor release sooner?