Skip to main content
OGaie
Associate II
August 21, 2019
Solved

USART Communication Nucleo-L4r5zi isn't working?

  • August 21, 2019
  • 1 reply
  • 911 views

I'm using the Nucleo-L4r5zi I can't send a receive a simple message using USART Communication,

Which pins to configurate on the Cube MX ? should i use an FTDI (usart to usb cable) ?

This topic has been closed for replies.
Best answer by Tesla DeLorean

This is the user manual for the board https://www.st.com/content/ccc/resource/technical/document/user_manual/group0/6e/c2/81/e8/92/5f/41/cc/DM00368330/files/DM00368330.pdf/jcr:content/translations/en.DM00368330.pdf

>>Which pins to configure on the Cube MX ?

The Nucleo's VCP is LPUART1 on PG7 and PG8, so you'll want to use that, enable power on the GPIOG IO bank, and make sure all the solder-bridges are in order.

>>should i use an FTDI (usart to usb cable) ?

Shouldn't need too

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
August 21, 2019

This is the user manual for the board https://www.st.com/content/ccc/resource/technical/document/user_manual/group0/6e/c2/81/e8/92/5f/41/cc/DM00368330/files/DM00368330.pdf/jcr:content/translations/en.DM00368330.pdf

>>Which pins to configure on the Cube MX ?

The Nucleo's VCP is LPUART1 on PG7 and PG8, so you'll want to use that, enable power on the GPIOG IO bank, and make sure all the solder-bridges are in order.

>>should i use an FTDI (usart to usb cable) ?

Shouldn't need too

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..